Part Number: LM3429 Tool/software: WEBENCH® Design Tools Hello, I am designing a driver for LED CMT2890 (Vf=54V; I=3.3A) using LM3429. The input: + VIN=12V + Vled=54V; I=3.3A. => Iswitch~20A. I tried to use WEBENCH but the tool does not support my case.…
Part Number: LM3429 Hi, It takes 30ms to start boost operation after input voltage to VCC pin (nDIM pin). Is it correct? Please let me know if there is any missing information. Best regards, Yuto Sakai
Part Number: LM3429 Hi, The nDIM pin has a threshold voltage of 1.24V and is described as Active low. (Described in Data sheet P.19 7.3.9) However, my customer says that it is enabled when the nDIM pin is "H". So, I would like to check the operation…
Part Number: LM3429 hi sir,
my customer use LM3429 to drive a 13.3 inch panel, now customer use a external PWM to Dimming , now customer wants to know what's MAX Frequency of PMW connected the pin 7(ndim),Tks.
Part Number: LM3429-Q1 Other Parts Discussed in Thread: LM3429 Dear Sir,
Greetings!
I need an immediate help in solving the issue with LM3429 for my design. The design details are
Vin : 10-15 VDC
Vout: 24-38VDC
ILED: 0.45A (typ)
Rlim - 0.075 ohm / 0.0…
Hi Lupillo,
You mention above' the board cannot be repaired no matter what you do'...Does this mean that you have tried replacing all the components on the board and it still does not work? When things failed how does it failed? I there any switching…
Part Number: LM3429 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Dear All,
I am simulating design for Time of Flight camera's illumination board. I am trying to replicate OPT8241-CDK-EVM design. My problem is that generated…
Part Number: LM3429 Tool/software: WEBENCH® Design Tools When a design generates a CUSTOM resistor or capacitor and an alternate is not available for the range of parameters, how would can I find a component to use. Also, when I click on Build-Lite and…
Part Number: LM3429 Other Parts Discussed in Thread: TPS92691 , TPS92692 Hi All,
I got a question from my customer: What's the maximum power that LM3429/TPS92691/TPS92692 are able to drive? And do we have any related materials on how to estimate or calculate…
Part Number: LM3429-Q1 Other Parts Discussed in Thread: LM3429 , TPS92692 Dear Sir:
Our customer would like use LM3429-Q1 for head light application. Does TI have reference design of LM3429-Q1 can meet Class-5 certification? Or Does TI have layout…