Part Number: LM3429 Other Parts Discussed in Thread: TPS92691 For a new project we are starting we need to control a polyamide heater pad with a maximum power of 160W 24V Hz. We have a temp sensor for measuring the temperature and a T.I. Piccolo DSP for…
Part Number: LM3429 Other Parts Discussed in Thread: LM5022
Hello, I am looking for a boost converter to convert 24V (BAT) => 80V to over-drive a LED array (Vf ~ 80V - If ~ 4.9A - rD = 3.56 Ohm) at pulse width of about 200us (f ~ 20Hz).
I have run some…
Part Number: LM3429 Other Parts Discussed in Thread: TPS92691 Tool/software: WEBENCH® Design Tools Design Constraints: Custom LED Vf=12.4V, If=1.05A, Rd=1.3ohm. 3-Series, 1-Parallel, Vinmin=8, Vinmax=32, Ta=30C (CREE XHP35)
Can someone run these constraints…
Part Number: LM3429 Other Parts Discussed in Thread: ABS , TPS92075 , TPS92074
Hello there,
I was thinking about adding a Zener diode/(Voltage regulator) to limit the VCC, and use appropriately rated components for the Buck-Boost configuration, so that…
Part Number: LM3429 Other Parts Discussed in Thread: TPS92515 , TPS92691 , TPS92692 Hi,
I am using LM3429 in my front Lighting design. But I saw the part No. is too old, do you have any suggest like LM3429 function ?
thanks.
Part Number: LM3429 Hi Team,
I saw LM3429 can program switch frequency setting off time via RCT component RT/CT, but has no recommend around minimum - maximum. Could you help provide switch frequency limitation?
Part Number: LM3429 HOW CAN I USE LM3429 FOR DIMMING PURPOSE?
MY REQUIREMENTS ARE:
IT SHOULD BE ON WHEN I PROVIDE PWM TO nDIM & SHOULD BE OFF ON PROVIDING THE SAME..
Part Number: LM3429-Q1 Other Parts Discussed in Thread: LM3429 Hi,
I'm designing a LED driver with the LM3429 as a boost:
Vin=12V.
Vo = 15 to 35V (typical: 29,5V).
Io = 0.4 - 1A. (analog dim with i2c digital potentiometer)
I don't quite understant…
Part Number: LM3429 Hello,
I've made some simulations with LM3429 and it worked fine. I had efficiency up to 93% with boost topology :D. But the problem is with exported files. I"ve exported both PCB layout ant schematics. PCB layout works fine with…
Part Number: LM3429-Q1 Other Parts Discussed in Thread: LM3429 , TPS92691 , TPS92690 , TPS92692 Usually how we design a π EMI filter and how to choose the size, value of the inductor and capacitors? Do we design the EMI filter before finishing the schematic…