Part Number: LM3447-PAR-230VEVM Other Parts Discussed in Thread: LM3447-A19-230VEVM Hi,
As per LM3447-PAR-230VEVM Schematic, rectified AC is connected to transformer pin no.1 and is connected to signal ground...
is it correct?? or transformer pin no 14…
Part Number: LM3447-A19-120VEVM Other Parts Discussed in Thread: LM3447 Hello,
I am testing the LM3447-A19-120VEVM evaluation board to check the performance with different triacs. The IC works well but has a one major issue which I am trying to resolve…
Part Number: LM3447-A19-230VEVM hello i was wondering if someone could explain me the unusual LC filtering configuration used in the emi filter. It resembles a 4th order LC filter but is placed across the ac input.
Hi Krupali,
This is a duplicated thread with LM3447-PAR-230VEVM: LM3447-PAR-230VEVM Schematic - Power management forum - Power management - TI E2E support forums
Let's continue the talk in that thread. I am going to close this thread.
Best Regards…
Part Number: LM3447-PAR-230VEVM I have bought LM3447-PAR-230VEVM. In the datasheet,
www.ti.com/.../sluua02.pdf
page 11, fig12, you show input current. But I have not obtained this current, The input voltage and current graph is in the following link…
Other Parts Discussed in Thread: LM3447-A19-230VEVM I'm designing LED driver for LED bulb 9W , Vout = 30V , I =275mA , f = 75Khz , n(efficiency) = 0.82
Input Voltage range : 190-265V , Pin =10W
I based on reference design LM3447-A19-230VEVM .
I bought…
The shape of the current is shown in the figure. This is the minimum level of brightness. We conducted tests on another load (15W) using LM3447-PAR-230VEVM. At the minimum dimming levels, there are also minor changes in brightness visible to the eye. As…
Hello Irwin,
In reality its not the transformer that is causing me the problem, its the massive capacitor on the primary side... if only it were on the secondary side there would be no issue.
I have seen other reference designs, for example, www.ti…