Part Number: LM3477 Tool/software: Dear TI Support Team,
We are facing an instability issue with our LM3477 buck converter design and would appreciate your guidance.
Application details:
Input voltage range: 23 V – 29 V
Output voltage: 14.9…
Part Number: LM3477 For a standard buck design, is the compensator network required as a default in the LM3477?
The datasheet mentions:
"With the power stage known, a compensator can be designed to achieve improved performance and stability. The…
Part Number: LM3477 Hi Team,
Our customer noticed that the feedback voltage of LM3477 is higher than the maximum value of 1.29V. According to our customer,
I have designed a board with a LM3477, and I have noticed that the feedback voltage on the…
Part Number: LM3477 hello,
Could you provide LM3477 external components calculation tool or spreadsheet ? Our customer encountered unstable output so he needs external calculation tool or spread sheet.
I have checked, but this device does not have…
Part Number: LM3477
Hi,
In an LM3477 Inverting Buck Boost configuration where the IC ground is negative voltage referenced and sinking current, what is the correct current sense configuration? In the buck configuration, the sense resistor is between…
Part Number: LM3477 Sir/Madam
I need the LM3477 part library having its .olb and .lib file for simulation purposes. However, it is not available on the ti website. Please provide the file asap.
Part Number: LM3477 Hi,
My doubt is related to the choosing appropriate value in R_sense calculation. (Page No.16 at the datasheet)
in R sense calculation,
I find Vcl(0)(min) and Vcl(0)(max)... how to choose those values??
Other Parts Discussed in Thread: LM3477 Dear,
we have an application where we use LM3477 as DC/DC from 12V (18-22V) sollar cell down to 4.4V.
Unfortunately 10-20% of our LM3477 have blown after weeks of good opperation. We do not know what we do wrong…
Part Number: TPS54J061 Other Parts Discussed in Thread: TPS62150 , LMR54410EVM , TPS62933 , LMR54410 , LMR14020 , TPS82130 , LMR70503 , LM3477 , TPS62130 , TIDA-01457 , TIDA-01405 Hi,
I'm trying to create an inverting buck-boost, as described in appnote…