Part Number: LM3478 Hi Team,
The POS boost uses the LM3478 in conjunction with the customer-supplied I/O board (24V). An abnormal sound is produced at 0A, which is currently believed to be caused by not entering CCM.
During customer recent experiments…
Part Number: LM3478 Hello,
Is it possible to design a 3V to 40V boost converter with an output power of 6W with the LM3478. I know it is a high duty cycle but is it possible?
Greetings Daniel
Part Number: LM3478Q-Q1 Other Parts Discussed in Thread: LM3478 Hello, good day. Our customer have a problem :
Does the lm3478 chip control the voltage loop and current loop together? For example, in this picture, during normal operation, if the input…
Part Number: LM3478 Other Parts Discussed in Thread: LM5155 Tool/software: Hi,
Q1. I believe that the variation in V_SENSE and V_SL ratio described in the Electrical Characteristics of the data sheet is temperature dependent, is this correct? Also,…
Part Number: LM3478 Hello,
Please help to review the design attached herewith with below mentioned power controllers.
LM3478MM/NOPB
TPS61236PRWLR TPS62865RQYR
schematic_for_review_ti_LM3478.pdf
Part Number: LM3478 Other Parts Discussed in Thread: LM5156
Greetings, I hope somebody could help me. I'm trying to design a SEPIC converter based on LM3478, with input voltage range 12-36V, and output 24V 2A. I'm calculated all relevant values of components…
Part Number: LM3478 Other Parts Discussed in Thread: LM348 Hi,
I am an embedded developer at Thornhill Medical, a company that makes life support devices for military applications.
We are currently using the LM3478 IC on of our product as a Flyback…
Part Number: LM3478 Hi,
In a booster circuit using lm3478 , The output oscillates when the load changes.
Vin is +24V ,Vout is +80V and 0.3A .
The circuit diagram and oscilloscope image are shown.
Please give me advice to solve this problem.
…
Part Number: LM3478 Hi,
Good day,
I am using LM3478 in buck boost config where my input range will be 10-15V and my output will be 12V and 2.5Amps max. In my current implementation the mosfet is heating and my whole board is heating for even for…
Part Number: LM3478 Other Parts Discussed in Thread: LM3481-FLYBACKEVM , LM3481 , LM5155 , LM5156 Hello, My customer wants to evaluate LM3478 for flyback topology. But we don't have any flyback EVM with LM3478. Then they think using LM3481-FLYBACKEVM…