Part Number: TLV760 Other Parts Discussed in Thread: TPS7B69 , TPS709 Hi all,
I am looking for a replacement for the LM3480IM-15NOPB, where I have found the TLV76015DB. Can you help assist me in determining differences between the two parts?
www.ti.com/…
Part Number: LM3480 Hello.
When I apply voltage to the LM3480IM3-15, the output from the regulator is turned on and off a couple of times before it stays at the wanted 15V. Vin ( and also Vout from regulator) ramps from 0V to 15V for approx. 20ms. Vin…
Part Number: LM3480 Hi, I have a LM3480 for supplying an µC from 12V. Because I want to use the 5V supply from the progger without any 12V supply I have an inverse Schottky diode across the (between in- and output) of the LM3480.
Unfortunately the…
Part Number: LM3480
The LM3480IM3-3.3/NOPB voltage regulator will not work in our test circuit with Vin above 16V. When Vin > 16V the output voltage begins to decrease to ~ 2.6V and current is limited to < 30mA. Ambient temperature was around…
Part Number: LM3480 Other Parts Discussed in Thread: UA78L , TPS7A25 , LM317L I'm looking for a regulator which can compete with MCP1702. The LM3480 can only support 100mA and not SOT89 package.Is there any similar product to compete?
application: Motor…
Part Number: BQ25703AEVM-732 Other Parts Discussed in Thread: LM3480 , BQ25703 Hello, I hope you are well, I am working on a custom PCB based on the BQ25703A-EVM, and I am a little confused about the power input to the 3.3v LM3480 LDO. According to the schematic…
Part Number: AMC1306E25 Other Parts Discussed in Thread: LM3480 , TIDA-00914 Hi Ti ,
In the circuit diagram of TIDA-00914, when the AMC1306 is used for current sensing, an LDO(LM3480) is employed between AVDD and AGND to serve as the power source for the…
Part Number: LM3480 Hi,
I am using a LM3480 on a board to generate a 3.3 V power supply with a 12 V power supply.
While testing several of my boards at 70°C, I have problems with some of them for which I was able to see on a scope the power output of…
Part Number: SN74LVC1G57 Dear Technical Support: Good day, We plan to use several of your IC devices, Please see attached EXCEL file,
We hope to know the following information regarding the fabrication of related ICs, Specifically, the technology nodes…