Part Number: LM3481 Other Parts Discussed in Thread: PMP10352 , , PMP Tool/software: Hi expert,
My customer used LM3481 and refer to the PMP10352 circuit for PoE 15W output application.
There is no problem to load 15W at output of LM3481 without main board…
Hi Zoe,
I received a mail request on this exact issue from your colleague Racheal. The response is summarized here:
Please note that the LM3481 has two protections for overcurrent events: - overcurrent protection (160mV threshold) - short-circuit protection…
Part Number: LM3481-Q1 Other Parts Discussed in Thread: LM3481 Hi team,
Below circuit is LM3481 external schematic. Customer feedback when 5Vout put drops down, the duty cycle remains the same.
CH1: RESET CH2: Vin CH3: DR CH4:5V out
CH1:Vgs CH2:Vr_s…
Part Number: LM3481-Q1 Hi Team,
Based on LM34xx How to Design Flyback Converter with LM3481 Boost Controller (Rev. A) (ti.com.cn) , my calculation of Lm is about 110uH as below.
VIN=32V Vout=12V. others are same as below.
However, in chapter 4, it says…
Part Number: LM3481 We want to the following Specifications:
Vin = 12V
Vout = 24V, 2A
V Output Control with PIO pins.
The circuit diagram we currently use is as follows.
PIO Control L(0V) = Vout 12V
PIO Control H(3.3V) = Vout 24V
We want the output…
Part Number: LM3481-Q1 Hi team,
This is Chloe, NWC AA2 FAE. There is an issue about small signal model derived. Such as Figure 6, write the KCL equation according to the last sequence of small signal circuits, and compare formula 14 to get the relationship…
Part Number: LM3481 Other Parts Discussed in Thread: LM5155 Hi,
Does LM3481 possible to using for below LED design? Seems it can't fix output current?
DC-DC LED Constant Current Waterproof Isolated Power Supply 200W Specifications:
Input Voltage Range…
Part Number: LM3481 Hi team. I've been working on the LM3481 SEPIC converter for a while now and it alwyas keeps on comin up with newer problems. Vin:18V to 30V Vout:24V/1A A coupled inductor design is being used and the DRQ125-220-R is being used as…
Part Number: LM3481 Hi team So i've been using the LM3481 for a sepic converter for a while and i have had problems with the board (Please refer to the previous thread: https://e2e.ti.com/support/power-management-group/power-management/f/power-management…