Part Number: LM3481-FLYBACKEVM Dear Sir/Ms.
How do I download the gerber of the LM3481-FlybackEVM? My customer wants the gerber file of the LM3481-FlybackEVM and they want to make their own board. would you give me gerber file?
Best Regards,
Kami Hua…
Part Number: LM3481-FLYBACKEVM Hi,
in our EVM, we have compensation capacitor and resistor on secondary side, and we have compensation capacitor and resistor on COMP pin,
is the compensation capacitor and resistor on COMP pin a must? Can it be replaced…
Part Number: LM3481 Hi Dear,
Can please anyone describe if I can increase the output current of the LM3481-FLYBACKEVM?
If the increase in current is possible then how much it can go above 2A with stable output voltage?
Kind regards
Mohsin
Part Number: LM3481-FLYBACKEVM Other Parts Discussed in Thread: LM3481 Hello all,
I have a question about the diodes D4 and D5 on the secondary side of the EVM. Can I ask why you put these diodes? What does these diodes do?
Thank you, RYO
Part Number: LM3481 Hello,
I am using this chip to control a flyback transformer, reference from LM3481-FLYBACKEVM. I read the spec sheet of LM3481 and discovered that even though there is Isen for the current control, there is still FB for voltage control…
Part Number: LM3481-FLYBACKEVM Other Parts Discussed in Thread: LM3481
Hello all,
I replaced R16 to 1kOhm in order to make the output voltage to 5V. Changing the output voltage, the phase/gain margin may change, so I measured those margin by FRA…
Part Number: LM3481-FLYBACKEVM Other Parts Discussed in Thread: LM3481 , Hello,
I would like to design a Flyback-Converter using the LM3481. I use the LM3481-FLYBACKEVM to test my design.
The specification is as follows: Vin = 5.4 to 17 V Vout = 6 V +/- 1% …
Part Number: LM3481-FLYBACKEVM Hello @TI teams,
Currently working on your LM3481-FLYBACKEVM testboard for my company, I'd like to tinker with its simulable schematic, using SIMetrix.
Is there a deposit where I'd be able to download such file? …
Part Number: LM3481-FLYBACKEVM Other Parts Discussed in Thread: LM3481 Hello all,
I've got the LM3481-FLYBACKEVM to use it as a testplatform for a LM3481-based Fyback-powersupply.
I changed the following parts: R13 from 162k to 105k (new switching…
Part Number: LM3481-FLYBACKEVM Other Parts Discussed in Thread: LM3481 , PMP10725 , , CSD19532Q5B , CSD19502Q5B , CSD19538Q3A Dear all.
I examine Flyback by LM3481. CSD19502Q5B and CSD19532Q5B are used for each of LM3481-FlybackEVM and PMP10725. These IDM is…