Part Number: LM3481-Q1 Hello,
We have a SEPIC design including the LM3481-Q1 controller.
According to the datasheet, Cin should be above 100uF.
However, the Powerbench suggests Cin to be tantalum 4.7uF.
The questions are:
1) Who should I follow…
Part Number: LM3481-Q1 Tool/software: Hi,
We made WEBENCH with the specifications that customers want.
6138.WBDesign86.pdf
The Rsense value is 2.46928 mOhm.
2.46928 mOhm is a custom specification, so I want to change it to a different value. …
Part Number: LM3481-Q1 Hi team,
This is Chloe, NWC AA2 FAE. There is an issue about small signal model derived. Such as Figure 6, write the KCL equation according to the last sequence of small signal circuits, and compare formula 14 to get the relationship…
Part Number: LM3481-Q1 Hi team,
I'm BCCing this thread to my customer. Could you tell me if you can provide the password for this calculator--FLYBUCK-FLYBACK-DESIGN-CALC? This is because they'd like to see how the result comes out. Specifically speaking…
Part Number: LM3481-Q1 Other Parts Discussed in Thread: LM3481 Please assist in confirming with the original Ti factory the control standards for the pin flatness of the accessory power supply IC (lm3481) and the means used to ensure and monitor it. …
Part Number: LM3481-Q1 Other Parts Discussed in Thread: PMP40100 Hi Expert, Wanted to know if the IC supports primary side regulation, if it is a yes I like to have the supporting documents regarding primary side control operation.
Part Number: LM3481-Q1 Hello community!,
I would like to have more insight on component selection and design considerations of LM3481-Q1 based flyback converter with 12V, 25W output. I have referred to the technical datasheets of LM3481-Q1 but I could…
Part Number: LM3481-Q1 Hi team,
What will happen if customer leave LM3481-Q1 pin FA/SYNC/SD floating? Can IC operates at certain fix frequency or it cannot work normally? Thanks
Scarlett
Part Number: LM3481-Q1 Other Parts Discussed in Thread: LM5155 Hi team,
May I know if you have below temperature-Vsense curve? 100mV and 190mV corresponding to Vsense under which condition? Thank you
Thank
Scarlett
Part Number: LM3481-Q1 Other Parts Discussed in Thread: LM3481 Hi team, from datasheet Duty cycle maximum is 85%. I want know what happen when we design Vin=5V,Vout=40V. is it Vout=33.33V or device not work, Vout=0V?