Part Number: LM34923 Other Parts Discussed in Thread: TIGER Tool/software: Hi Team,
Could you please let me know the Rjc(top) spec for LM34923?
Thanks and Best regards,
Tiger
Part Number: LM34923 Other Parts Discussed in Thread: LM34927 , LM5169 , LM5163 Hi Team,
Is there a corresponding next-generation product for LM34923?
If so, please share the relevant slides with me. Thanks.
Regards,
Charlie
Part Number: LM34923 Has anyone used this regulator for negative voltage regulation. I need a pre-regulator for + and - voltages. About 30V and -30V out at less than 0.5A. The inputs can be somewhere between +-65 and +-40V. I like this device for the…
Part Number: LM34923 Hi Team,
In the datasheet, there is only the thermal resistance between the die and the environment. What is the thermal resistance between the die and the case? Thanks.
Regards,
Charlie
Part Number: LM34923 Other Parts Discussed in Thread: LM5006 Hi Team,
A customer wants to confirm if there are other difference between LM5006 and LM34923 aside from the LG pin which is intended for synchronous rectification.
Regards,
Danilo
Part Number: LM34923 Other Parts Discussed in Thread: TIGER Hi~
Currently, the test waveform showed the negative pulse of SW to RTN is less than -1V.
There is no specified transient spec in the absolute maximum rating. Only steady spec to -1V in minimum…
Other Parts Discussed in Thread: LM34923 Hello,
what ist the maximum inrush current of the LM34923 @48V Vin or, how can I determ it?
Best regards
Michael
Other Parts Discussed in Thread: LM34923 Dear all.
Can LM34923 use an inductor of 22uH in the following condition? Input=48V; Output=12V-0.5A
Regards, PAN-M
Other Parts Discussed in Thread: LM34923 Dear all.
Do you have any thermal registance of LM34923? (θJCtop, ψJT) Is 200°C/W of θJA correct?
Regards, PAN-M