Part Number: LM34927 Other Parts Discussed in Thread: LM5017 , Dear Team,
What is the reason we need the diode here?
The datasheet mention it will be optional in the 8.2.1.2.13, but it didn't explain what is the pros and con.
Beside, what is the different…
Part Number: LM34927 I use the LM34927 to converter 24V to 12V to drive the 16pcs relays. The relay core resistance value is 240Ω. So the output current of 12V about need to 711mA. And I check the datasheet of the LM34927 in page6 has the current minimum…
Part Number: LM34927 Other Parts Discussed in Thread: LM5161 I want to use LM34927 to converter Input voltage 24V to output voltage 12V. The output just to drive the 16pcs relays. Every relay core resistance has 270Ω . So I calculate output current about…
Part Number: LM34927
Hi Sir,
My customer is using LM34927 as aux power controller of their DC/DC bricks. The testing input voltage is 50V and other parameters/output loads are shown below.
They want the VOUT1 to be 10.5V , so they choose the feedback…
Part Number: LM34927 Other Parts Discussed in Thread: LM5017 , I am currently using lm34927 however I have seen an app note using an LM5017 What Are the basic differences of these two parts .Basically designing dc dc 12 0 12 isolated buck convertor
Part Number: LM34927 Hi
in LM34927 datasheet, when Icc=20mA, the max VCC is 8.55V
but in below circuit, the ICC will be 0mA at normal operation
so customer want to know when ICC=0mA, what's the max VCC voltage?
thanks.
Part Number: LM34927 Hi Team,
My customer now is evaluating LM34927 for buck control, which used external VCC power supply and VCC kept as 11V, while the VCC > VIN, the power consumption would increased to 0.6W which is out of spec. could you kindly…
Part Number: TPS54824 Other Parts Discussed in Thread: LM5117 , LM5576 , TPS543C20A , LM5069 , LM34927 , TPS62125 Team,
Currently my customer is using TPS54824 on their board, we have some questions about the EN pin spec. Could you please help with it?
…
Part Number: LM5169-Q1 Other Parts Discussed in Thread: LM5168-Q1 , LM34927 Hi Team,
I have a customer who is interested in using LM5169-Q1 and were curious about the current limit.
From the data sheet, it mentions that the current limit is 0.7A while…
Part Number: LM5169-Q1 Other Parts Discussed in Thread: LM5168-Q1 , LM34927 , LM5169 Hi Team,
I have a customer who is interested in using LM5169-Q1 and were curious about the current limit.
From the data sheet, it mentions that the current limit is 0.7A…