Part Number: LM34936 Other Parts Discussed in Thread: LM5176 Hi,
I have 2 questions in addition to the threads of Tyhran a few months ago (high voltage DC/DC converter with LM34936), we are working in the same team.
1. The real ranges are: Vin = 10..…
Thank you so much Stefan! I have used the excel macro tool you suggested, and here is the circuit now.
Could you take a look and check if there is something i need to change?
Clas
LM34936 Buck-Boost Quickstart Tool 2024 FEB 25.pdf
Today we probably resolved the problem by ourselves: We found that the high side gate driver output of the LM34936 doesn't send any switching signal to our external gate driver IC LM5108. The origin for this seems to be the fact that the BOOT pin of the…
Part Number: LM34936
Hi!
Question about CC mode implementation
Concept for Constant Current mode: ISNS+ and ISNS- is used to achieve current feedback control ISNS- voltage is controlled by PWM signal. ISNS+ voltage comes from current shunt IC. Current shunt…
Part Number: LM34936 Other Parts Discussed in Thread: LM2105 , Hello TI team.
I want to use LM34936RHFR in my application.
It is buck-boost convertor with high input voltage and high Power (600 W)
Specs:
Vin: 30-85V
Vout: 52V 10A
In addition to standard…
Part Number: LM34936 Hi support team, Please let me know the meaning of VBIAS(SW).
Does it mean that BIAS input will not be accepted when TYP is less than 8V? Or does it mean we need an 8V input to generate 7.35V for VVCC(VIN)?
I would like to confirm…
Part Number: LM34936 Hi support team, Continuing from the "Original question" above.
What conditions require the BIAS pin to be energized? Please let me know the conditions of VIN, etc.
Regards, Dice-K
Part Number: LM34936 Other Parts Discussed in Thread: CSD19502Q5B , CSD17303Q5 , CSD18513Q5A
Hi,
We are considering the circuit configuration shown in the attached image. Could you please check if there are any problems with the constants of the peripheral…
Part Number: LM34936 Other Parts Discussed in Thread: LM5175 , LM5176 , ,
Hi support team,
What would be the recommended handling if the BIAS pin is not used? According to WEBENCH, it is connected to GND via 0.1μF. Shouldn't it be directly connected to…
Part Number: LM34936 Hi support team,
Do you have any plans to release a buck-boost module with a built-in inductor that can output 12V as shown below?
Vin: 10~18V Vout: 12V Iout: 3~4A
My customer was considering the LM34936, but decided to use another…