Part Number: LM34936 Hi support team,
Should BIAS be connected to VOUT when used under the following conditions?
Vin: 10~17V Vout: 12V Iout: 3~4A
If so, is a diode on VIN unnecessary?
Regards, Dice-K
Part Number: LM34936-Q1 Hello,
I designed a buck-boost using LM34936-Q1. I am noticing that the output ripple has weird shape ( attached).
I measured SW jitter, Bode plot. Everything is fine. Jitter less than 3% and Phase margin > 80 degree, BW = 25kHz…
Hello John,
I have not seen an update on this thread for the last 11 days.
Maybe you could solve this issue already in the meantime, in this case it would be great to press the is solved button.
If there is still something open, just let me know with…
Part Number: LM34936 Other Parts Discussed in Thread: TPS65987DDJ
Hi Sir,
My customer would like design two LM34936 in Dell new two type C port monitor project.
Would you please review schematic and provide your comment?
https://txn.box.com/s/9ual9…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM5175-Q1 , LM5152-Q1 , LM5176 , LM34936 , LM5175 E2E,
My requirements:
1. AEC-Q100 rated,
2. VIN range: 7.5 to 12.6V
3. VOUT = 12V (fixed)
4. IOUT = 6.27 A max
5. Part must have a working PSpice model…
Part Number: LM34936-Q1 Hi team,
Customer is going to use LM34936-Q1 with below Vin ripple condition.
Vin : 21V
Input ripple voltage : 600mVp-p
Ripple frequency : 400kHz
Is these ripple no problem to the device behavior?
Because Figure 8-1 in the datasheet…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM5176 I started with the LM5176 design spreadsheet and the WEBench design: https://webench.ti.com/power-designer/switching-regulator/customize/18?noparams=0
I tried to include the schematic below…
Hi, Sorry for the delay. I did finally switch to another chip, the LM5118, and everything is working smoothly now. Thanks for you time anyway. Regards, Arthur
Part Number: LM34936 Hello Experts, My customer ask about a following question. Would you answer it? [question] If the external high side FET(output) is shorted accidentally and then the external low side FET is enabled(it will flow a short through current…
Hi Anushree,
I have not seen an update on this thread for the last 24 days.
So I assume the issue is solved.
In this case it would be great to press the is solved button.
If there is still something open, just let me know with the new details.
Best…