Hi Eng Lih Khaw,
Thanks you for reaching out with your question and for using the LM34936 in your design.
Here are my comments regarding the schematic.
1. SLOPE capacitor (C12)
I suggest decreasing this resistor to 180pF. This will increase the…
Part Number: LM34936 Hi,
We're using LM34936 to generate 5V/9V/12V/15V/20V as PD source, and by default DITH pin is connected to GND through a 22nF cap. With such DITH connection, we can hear @ 5V and 9V out, but didn't hear it @ 15V/20V out. After…
Part Number: LM34936
The Simulation Setting is as the picture shows.when i run the simulation,The command line window is shown,"WARNING(ORPSIM-16534):Using high values of ITL4 for Speed Level",and the progress bar is still zero present.I want to know…
Part Number: LM34936 Hey there,
I'm working on a buck-boost design utilizing the LM34936 with the following parameters:
Vin: 6-26v
Vout: 12v
Iout: 5A
It's a pretty standard setup, pretty much all of my component values came from Webench…
Part Number: LM34936 Hi,
I am looking for a part which supports the below requirements. Can LM34936 support the load current?
Input:
DC 8 V - 20 V
Output:
14 V at 12 A
Temp:
30 °C
If not what is the maximum load current with…
Part Number: LM34936 Hi Team,
would you please provide the comparison table to me?
https://e2e.ti.com/support/power-management/f/196/t/762581?tisearch=e2e-sitesearch
BR,
SHH
Part Number: LM34936 Hello,
I am working with the LM34936QPWPTQ1 IC following a WEBENCH example for a 12-36V input Buck/Boost converter with 28VDC/8A output. I am currently testing a board design that I made and am not getting the desired output voltage…
Part Number: LM34936-Q1 Hi Ti staff,
I found the 10 Ohm resistor connect series at Vin PIN of this ICs. I can not find the reference for what the propose of this resistor. 1- Could you tell me why this resistor is connected in your reference schematic…
Part Number: LM5176 Other Parts Discussed in Thread: LM34936 , Hello,
Apart from pinout, can someone tell me the fundamental differences between LM34936 and LM5176 buck-boost converters?
Thanks.
Regards. Matthieu