Part Number: LM34936-Q1 Hello,
I designed a buck-boost using LM34936-Q1. I am noticing that the output ripple has weird shape ( attached).
I measured SW jitter, Bode plot. Everything is fine. Jitter less than 3% and Phase margin > 80 degree, BW =…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM5176 , LM5176-Q1 , LM34936 , We have a design that uses the LM5176-Q1. Our input voltage is 24V. Is LM34936-Q1 a drop in replacement for this design? Also, is there a Quick Start Tool spreadsheet…
Part Number: LM34936-Q1 Hi team,
Customer is going to use LM34936-Q1 with below Vin ripple condition.
Vin : 21V
Input ripple voltage : 600mVp-p
Ripple frequency : 400kHz
Is these ripple no problem to the device behavior?
Because Figure…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM34936 , LM5170 Hi,
i need information for the below queries
1.we need buck boost controller for high power rating , please find the below voltage and current rating .
VIn=6 to 36V
Vout…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM5175-Q1 , LM5152-Q1 , LM5176 , LM34936 , LM5175 E2E,
My requirements:
1. AEC-Q100 rated,
2. VIN range: 7.5 to 12.6V
3. VOUT = 12V (fixed)
4. IOUT = 6.27 A max
5. Part must have a…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM34936 Dear TI
I search 4sw buckboost device from power source(solar, generator 12v) to Li battery 12v.
i want to develop a analog control (standalone) devices.
I am reviewing the lm34936…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM5176 I started with the LM5176 design spreadsheet and the WEBench design: https://webench.ti.com/power-designer/switching-regulator/customize/18?noparams=0
I tried to include the schematic below…
Part Number: LM34936-Q1 Tool/software: WEBENCH® Design Tools Dear all, for your kind help
This is my first design using WEBENCH
webench.ti.com/.../SDP.cgi
While on the bοοst mode
Q3 & Q4 keep blowing
Any ideas?
LM34936QPWPRQ1.PDF
Part Number: LM34936-Q1 Hi Ti staff,
I found the 10 Ohm resistor connect series at Vin PIN of this ICs. I can not find the reference for what the propose of this resistor. 1- Could you tell me why this resistor is connected in your reference schematic…
Part Number: LM34936 Other Parts Discussed in Thread: LM5176 , LM5175 , , Hello, I need Pspice model to simulate this part LM34936 / LM34936-Q1 / LM5175 / LM5176
the Pspice in website is encrypted. Thank you