Part Number: LM34936EVM Other Parts Discussed in Thread: LM5176 Tool/software: To configure the LM34936EVM converter for 12 V input and 24 V output at 8 A load current, some modifications were made to the board: the sense resistor (R10) was changed from…
Part Number: LM34936EVM
Input is 12 V and output is 24 V. To achieve the 24 V output, I changed R14 to 20 k ohm and R19 to 560 kohm. However, I observed that the input current at no load is about 0.09 A, whereas it should be 0 A. Could you please help…
Part Number: LM34936EVM Other Parts Discussed in Thread: LM34936 Tool/software: Dear e2e support,
Could you clarify the role of the RC networks R8, C17 and R5, C7?
Can we remove it from any kind of design/use case?
Regards,
Part Number: LM34936EVM Other Parts Discussed in Thread: CSD19502Q5B Hi,
Do you have any evaluation board that fits the specification below: 22-30V DC to 19.5V DC up to 14-15A.
Kind regards,
Bright
Part Number: LM34936EVM Hi
Please can you provide the CE/EU Declaration of Conformity for LM34936EVM ?
The product is CE marked but the CE/EU Declaration of Conformity is not available on the T.I website,
Thank you
Chris
Part Number: LM34936EVM Hi support team, Continuing from the "Original question" above.
D4 and D5 needed the same withstand voltage as the MOSFET. Should D4 match the Q1 rating and D5 the Q2 rating?
Regards, Dice-K
Part Number: LM34936EVM Hi support team,
The withstand voltage of D4 and D5 is 100V, but under the following usage conditions, is it okay if the withstand voltage is low (about 30V)?
Vin: 10~17V Vout: 12V Iout: 3~4A
Regards, Dice-K
Part Number: LM34936EVM Other Parts Discussed in Thread: LM34936 Hello, can I get these files as well? I am trying to avoid a 6 layer board. I don't see in the eval board documentation how the CS/CSG lines are not crossing the SW lines.