Part Number: LM35 Hi I am using LM35 precision centigrade temperature sensor in our 32A dc controlled three phase AC Solid state relay. Just while running the temperature rise test hooked up to picolog to find the temperature rise. one of the temperature…
Part Number: LM35
Hi everyone,
I was prototyping a design using a LM35 that I got from what i thought was a trusted source and couldn't get it to work right. The output was erratic although i was following the straightforward datasheet from TI. Despite…
Part Number: LM35 Dear Sir/Madam,
One of my customer observed the recent LM35DZ/NOPB part that they order is having slightly different lead finish. And I check the last PCN was issued in AUg 2018.
If there any latest issue of PCN for TO92 package which…
Part Number: LM35LM35CZ/LFT4-Texas Instruments-SENSOR ANALOG -40C-110C TO92-3
What is the Lifecycle status? Is Obsolete please provide the PCN/PDN with the LTB date.
What is the REACH status? Please provide the REACH COC.
What is the ROHS status? Is…
Part Number: LM35 bonjour,
dans nos station nous utilisons les LM35DZ pour mesurer la T° interne du site via un module ADM6017 qui des entrées analogiques
de maniere generale je n'ai jamais eu de soucis
en revanche on m'a demander d…
Part Number: LM35 Hi,
Is there any data or document which states that the output of one LM35DZ cannot be connected to the output of another LM35DZ?
I appreciate your help.
Thanks.
Kind regards,
Jerry George
Part Number: LM35 Other Parts Discussed in Thread: TMP235 , LM70 , LMT01 , TMP117 , Hi Team,
Please let me know, is the part LM35CZ/NOPB suitable to use as cold junction compensator IC?
If yes, I didn't see a description in datasheet of the IC being used…
Part Number: LM35 Other Parts Discussed in Thread: TMP235 , LM335
I want to know the output voltage in the circuit of FIG.
Looking at other threads of LM35, it was written that the output voltage can be expressed by the following equation.
Vout = 10mV…
Part Number: LM35 Other Parts Discussed in Thread: TMP235 , , LM235 I wish to use this part to read temperatures between about -20C and +80C. The data sheet, page 16, figure 18 shows the use of diodes to produce a negative reference. I have read the two…
Part Number: LM35 Hi,
My name is Jerry George and I work with a inverter design company in Melbourne, Australia.
We are using two LM35DZ temperature sensors in our power modules but when we run the end of line tests it shows as high temperature alert…