Other Parts Discussed in Thread: LM350A Hi,
Do you have the waveform of the output voltage starting up and Falling down on LM350A and LM237KC?
It is helpful that each times are about 1 sec.
My customer hopes to confirm the each waveform.
Thanks…
Part Number: LM350-N Other Parts Discussed in Thread: LM350A , LM1085 Hello TI experts,
My customer considers LM350 for their new product, instead of DCDC buck converter.
The application is medical equipment, so they are very sensitive to switching…
Hi Daniel,
the operating range is as listed on the front page and operating range of the datasheet.
It is -40C to +125C for the LM350A and 0C to +125C for the LM350.
Since all we offer now is the LM350 and not LM350A, the parts are rated at 0C to…
Hey Steve,
I looked for devices with current limit adjust capability with a lower Theta-ja:
https://www.ti.com/product/LM350A
https://www.ti.com/product/LM317A
https://www.ti.com/product/LM338
https://www.ti.com/product/LM1086
Could any of…
Hi Shai,
The LM150/LM350A/LM350 and LM1086 are some of TI's wide input linear regulators than can be used as constant current regulators without an external MCU. See the figure below for an example circuit. The output current is calculated as follows…
Part Number: LM317 Other Parts Discussed in Thread: LM2991 , LM337 , , LM350-N , LM350A , TPS7A33 , TPS7A47 , LM2941 , LM2941C , TPS7A39 Hello,
This is my first post. Ignore anything in my profile, i have overall archietcture and design responsibility…
Other Parts Discussed in Thread: LM350A What is the operating temperature range of the LM350AT? The SNVS772B –MAY 1998–REVISED MARCH 2013 datasheet says −40°C to +125°C in the Absolute Maaximum Ratings table on page 2 (and also on page 1) but says 0°C…
Part Number: LM350K STEEL/NOPB (unable to select) Other Parts Discussed in Thread: LM1084 , LM1085 , LP3856 , LP3873 , LM138 , LM338 , LM323-N , LM350-N
Dropout voltage of LM350K STEEL/NOPB @ 3A output current.
whats the minimum voltage i can give…