Part Number: LM3530 Hi,
I used the LM3530 for my display LED driver. I produced 8 pieces and 2 of them working fine. In other 6 PCB, I have the same voltage from SW pin to OVP. On normal PCB, the OVP pin voltage is 40V. But here I measure the same voltage…
Part Number: LM3530 When resetting the IC - what is the minimum hold-time, low, to reset the device?
i.e. I pull the HWEN pin LOW... but for how long?
Also - once I pull the HWEN HIGH for normal operation - how long should I wait before starting I2C communications…
Part Number: LM3530 Other Parts Discussed in Thread: LM3697 , LM3630A Hello,
My customer would like to use LM3530 due to I2C control, but there is no EVM.
Is there similar device to LM3530 which has EVM?
Best regards,
Katsu
Part Number: LM3530 Hi Team, According to the following specification, I believe HWEN pin should be applied down to 0V to reset wthout fault over the full operating ambient temperature range. Is my understanding correct? Best Regards, Yaita / Japan disty …
Other Parts Discussed in Thread: LM3435 If I want to write the lm3435 driver which chipset's driver sample code can I refer to design or there is other chipset I can use.
Other Parts Discussed in Thread: USB2ANY Hi
These software couldn't work without the DELL PC.
We were install this software to HP, Lenovo and so on, but not work.
Is it correct?
PAN-M
Part Number: LM3530SW-LINUX Other Parts Discussed in Thread: LM3530 , Hello team,
My customer has a question about kernel start up error in Linux driver of the LM3530 into Linux4.14.98.
My predecessor asked the same question in the link below, but it's…
Part Number: LM3530SW-LINUX Other Parts Discussed in Thread: LM3530 Hello,
My customer is implementing a Linux driver of the LM3530 into Linux4.14.98.
The device driver define in Kernel configuration, and describe the LM3530 in device tree as below. But…