Part Number: LM3555 Hi,
I am currently working with the LM3555 device. After implement the HAL in a microprocessor to handle this device I have realized of the following information which also appears in datasheet : " In I2C control mode, the end of…
Part Number: LM3555 Other Parts Discussed in Thread: LM3643 , LM36010 , LM36011 , LM3644 , Hi,
customer found they cannot configure the OEN bit to 1 through I2C. they tried to change other bits in control register, it's OK.
can you help to give suggestion…
Other Parts Discussed in Thread: LM3555 Hi
Can we set 55ms pulse width and 1/10 duty about LM3555? This is the request of LED.
The flash timeout duration is written to the datasheet that is 100 ms. Is this saying that 200mA continuous current among…
Other Parts Discussed in Thread: LM3553 Hi
Our customer need 180mA flash current (20mA Torch) setting, but this device set limiting minimum 200mA. Can we lower current setting by external circuit?
ex.
Regards, PAN-M
Hi,
I've attached the 2013 User's Guide for power products. Starting on page 53 you will find a selection of PWM controllers. many of these teh frequency can be varied according to external criteria.
As an example if you use a UC3842 it is a simple…
Gary,
Most any of our power controllers with dual output capability will provide the control. See attached document starting at page 50 with the dual output controllers on page 53 and 54 and choose what features you want.
Regards,
John