Part Number: TL082-Q1 Other Parts Discussed in Thread: LM358B Hi all,
My customer is experiencing an issue where the oscilloscope test on the -VIN end of TL082-Q1 has an interfering waveform, the -VIN end test on the LM358B does not, and the solution…
Part Number: LM358B Other Parts Discussed in Thread: TL431 , LM358 Hi,
Any one please suggest High and Low Voltage Cutoff Application Note
Which option is better A) LM358, B) TL431 ???
I need with high Accuracy and Precision
Part Number: LM358B Other Parts Discussed in Thread: TPS61094 Hi, this is the first time I have to solve this type of issue os summing 3 independent voltages with the common ground before an LDO. I'm trying to add 3 voltages, each one with a different…
Part Number: LM358B Hi experts,
We received LM358BIDR with MSL Level 2. TI.com shows this with a MSL Level 1. Digikey indicated them as MSL Level 2. There's no PCN on your public domain. Can you confirmed that MSL were previously MSL 2 and kindly share…
Part Number: LM358B Feedback about 1% defects in IC,OP Amplifier,SMD,SOIC-8,LM358BIDR,TI manufacturing process:
When the MCU panel UA08 IC uses LM358B to adjust the voltage to the maximum voltage of 14.5V (with full load), the output voltage is low ripple…
Hello Carolina,
Yes, LM358B is enough low cost. They can use it. but they ideally want to use lower offset voltage drift and lower offset current drift than LM358B. TLV9352 looks like relatively low cost and the offset voltage drift is lower than LM358B…
Part Number: LM358A Other Parts Discussed in Thread: LM358B , LM358 , The offset voltage of the LM358 shows only have positive value 3mV max, but the LM358B shows have negative and positive value, +/-3mV. My question are,
Is the LM358A only have positive…
Part Number: LM358B Hi team,
Could you share material content report of LM358BIDER with PCN#20210212001.1 change ?
We’ve requested it to TI CSC with request number#CS0434694, however no response.
We need the report to get an approval on the PCN…
Part Number: LM258A Other Parts Discussed in Thread: LM358B , LM358A , LM358 , LM258 Hi Amplifier Expert,
I have a design using LM258A, generally speaking, is LM358A or B a drop-in replacement. is there any trick or concern if I use LM358B? I notice that…