Part Number: LM3648 Other Parts Discussed in Thread: LM36010 , LM2759 Hi Sir,
If the LM3648 is in thermal shutdown, even if the die temperature is lower than 150°C, the LM3648 is not available for operation until there is an I2C read of the Flags1 Register…
Other Parts Discussed in Thread: LM36010 Dear Technical support
I'm looking for an infrared led driver
Here is my need :
From a 10ns pulse input (3.3V - 0V), I need to drive an infrared diode.
Forward voltage range of this diode is between 1.1V…
Other Parts Discussed in Thread: LM36010 , TPS61500 Hi TI experts,
today I am using TPS63802DLAR as a constant current LED Driver,
I have some problems with LED disconnection that burn the TPS driver.
I want to start a fresh design and look for…
Hi Sir,
I would highly recommend LM36010 for this application if the Vout not exceed 5V. LM36010 supports IR mode which can be triggered very quickly.
BR
Sean
Other Parts Discussed in Thread: LM36010 , TPS92200 Hi, support team
My customer has the questions as follow:
I'm looking for a LED Driver for a single high brightness LED (1,5A, 3-3,5V). The source is a single Li-ion Cell (3-4,2V). The driver should…
Part Number: LM3648 Other Parts Discussed in Thread: LM36010
1,Could you please help me find out how to c alculate the junction temperature or temperature rise of LM3648?The customer wants to know the upper limit of the ambient temperature to avoid…
Part Number: TPS60252 Other Parts Discussed in Thread: TPS92200 , LM36010 With an input voltage of 3.55 to 4.2V, can the TPS60252 control a single white LED on one channel with 3.1Vf and 20mA?(on a DMx input.). This is a LCD backlight application
It…
Hi Jimmy,
Could you share me the output load specification? How many LEDs at the load side?
If you just want to drivre one LED, I would suggest with the LM36010 first.
BR
Sean