Part Number: LM3644 Other Parts Discussed in Thread: TPS92201 Hello Expert,
Is there a way to keep ON at FLASH and IR MODE regardless of TIME OUT?
Isn't it possible?
Best Regards,
Michael
Part Number: LM3644 Regarding the LM3644YFFR LED driver, would you like to confirm if it is our main control unit that can be disconnected from the B2/C2/C3/D2 pins, And completely using I2C for control?
The specification states that the function of LM3644…
Part Number: LM3644 Other Parts Discussed in Thread: TPS922055 , TPS923655 Hi Dear,
The customer is looking for Illumination LED drivers, which are industrial cameras. The specific requirements are as follows“”
3A or above driving current,…
Part Number: LM3644 Hi team,
if Vin=0, Vout is high, can LM3644 block Vout to go into VIn?
from datasheet, the sync MOS is a PMOS, body diode is from SW to Vout, then it should be able to block the voltage from Vout into Vin. Is it right? thanks.
BR…
Part Number: LM3644 Hi I want to drive LM3644 using MCU. My strobe signal from Camera is connected to LM3644.
TX Pin diasbled 0
Strobe type 0
Strobe enable 1
Torch pin 0
Mode IR drive 01
LED2 off 0
LED 1 ENABLE
0x25 my enable register value. There is…
Part Number: LM3644 Other Parts Discussed in Thread: TCA9548A Hi Team,
I am looking for a simulation model of LM3644. Do we have any available for Pspice of TINA? I found no available in TI.com. I was wondering if there is any available on your side.
…
Part Number: LM3644 Hi,
I would like to use LM3644 to strobe VCSEL at its typical If=600mA. In this condition the VCSEL's Vf=2V.
1. Is LM3644 suitable to drive a LED/VCSEL with Vf lower than 2.3V?
2. What is the lowest Vf supported by this IC?
I found…