Hi Eli,
Schematically your question regarding bypass cap and input connection is basically fine. However your concerns of interference is really real if layout was not done correctly or optimally. In these buck converters, the Power pin is very noisy…
Part Number: LM3674 Other Parts Discussed in Thread: LM3671 , LM3670 Dear team,
the device is used in multiple designs and so far the -30°C was OK. There is a new request for going down to -40°C. Ideal the customer could reuse an existing design and therefor…
Hi Jason,
I'm attaching an updated .bxl for the LM3670. It should be live in the product folder in two days or less. I hope this solves your immediate problems, and that you are happy with the support we've provided to correct the issues you have…
Hi
Can I use LM3670 ? however, the datasheet says it is suitable for one Li-ion battery or 3 NiMH/NiCd batteries. Want to know whether it can be used for 3 AA Lithium batteries like L91?
Thanks
Heng
Other Parts Discussed in Thread: LM3670 My customer Alltek Marine using LM3670MFX-ADJ in Search and Rescue GPS, LM3670 operating ratings: 2.5V ≤ VIN ≤ 5.5V, but i measured peak over 5.5V in scope, my customer want clarify:
1. VIN Pin Absolute Maximum…
Hi, FD,
What is the output range for the LM3670 adjustable voltage options? in the datasheet, there is no such range description. But at page 13, it has description that "For any output voltages below 0.7 and above or equal to 2.5V, a pole must also be…
Other Parts Discussed in Thread: LM3671 , LMR10510 , LM26480 , LM3370 Hi,
I am wondering if the LM3671 is still an active part with no plans to EOL?
My customer is doing a board spin for cost-reduction and is wondering if they should switch to a newer device…