Part Number: LM385-2.5 1. Can you describe how use LM385, what's the input voltage range?
2. How to choose the pull up voltage and resistor? Can we change P5V to 3.3V and get the stable 2.5Vref out?
.
Part Number: LM185-2.5-N Hi Team, I would like to confirm if LM185H-2.5/NOPB can be a direct replacement for LM185BXH-2.5? I cannot see any more information for LM185BXH-2.5 so I cannot tell if LM185H-2.5/NOPB can be considered a direct replacement for…
Part Number: LM136-2.5-N
Hello,
I'd like to know input voltage range of LM136-2.5N.
Is it only necessary to satisfy the operating current(400uA to 10mA) using a serial resistor regardless of the input voltage range? Or should I consider the input…
Part Number: LM136-2.5-N Can anyone tell me the difference between P/N LM136H-2.5, LM136H-2.5/NOPB & LM136H-2.5/883? And the difference between the "AH" as well on all three. Thanks, Matt
Part Number: LM385-1.2-N Hello all,
For the LM336-2.5N and LM385-1.2-N packages can you verify if the pins start from( left to right 1 2 3) or (right to left 3 2 1)
The package outline drawing is a little confusing, link below:
http://www.ti.com…
Part Number: CC3135 Other Parts Discussed in Thread: WL1807MOD , WL1837MOD Hi Team,
Do we have suitable WIFI for dual 2.5/5GHz and support 802.11 a/b/g/n/ ac ?
Other Parts Discussed in Thread: TL431 Not sure is this is the correct forum to post this query in so apologies in advance if not.
I need a 2.5V reference for my PIC 16F886 project to act as a voltage reference for the Analogue/Digital converters built…
Part Number: LM4050-N-Q1 Hi,
I am using LM2050AEM3-2.5 for my application, Hence I want to simulate the behavior of Reverse Breakdown Voltage(±15mV) Tolerance for an Extended temperature range with the test circuit mentioned for Startup Characteristics…