Part Number: LM3880 Other Parts Discussed in Thread: LM2941 , If the LM3880 is configured such that its VCC pin is supplied with +5V (generated from a +12V input via an LM2941) and its EN pin is supplied with a voltage derived from the +12V input via…
Part Number: LM3880 Team,
I have a customer with the following question.
Do the timers run continuously or do they power up and start the timer when the enable signal is enabled or disabled?
Thanks,
Aaron
Part Number: LM3880 Hello,
The customer requires the following product information, the chip model is LM3880MF-1AA/NOPB, please help provide it. Thanks.
Name and address of wafer fab.
Name and address of chip packaging factory.
MOQ
SPQ
Capacity…
Part Number: LM3880 Dear Team,
My customer is considering to use the LM3880 in their application, and is checking the behavior of sequence operation. 7.3.2 Incomplete Sequence Operation in the datasheet describes belows, - This state only occurs if…
Part Number: LM3880 Dear Team,
Could you please provide the IBIS files for the following components?
LM3880MF-1AB/NOPB
We would appreciate it if you could share the files at your earliest convenience.
Thank you for your support.
Part Number: LM3880-Q1 For LM3880-Q1, please share the logic levels VIH and VIL for enable pin and FLAG out pins VOH. For FLAG out pins VOL is provided as 0.4V in datasheet.
Part Number: LM3880 Dear Sir/Ma'am,
I would like to know whether the LM3880 can be used as a power sequencer for an RFSoC Gen3 device. If it is suitable, could you please share any relevant application notes, reference designs, or documentation?
If…
Part Number: LM3880-Q1 Hi Team,
We have used the LM3880QMFE-1AA/NOPB in a couple of our designs. During testing, we observed that FLAG 2 does not appear to follow the timing recommendation specified in the datasheet.
Please find our schematic below…
Part Number: LM3880 Dear Forum,
I need the EN pin to react to short 10-100us glitches. I noticed in the PSpice model that when I connect Flag3 with a diode to the enable pin that the glitch is recognized an I can use Flag 2 with a proper time delay…
Part Number: LM3880 Tool/software: Over two months ago I asked the following question and never received a response. Help, please!?
I have two circuits that are pretty much identical in pspice, and I'm getting very different results. For example, in…