Part Number: LM3880 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Is there a TINA simulation example design available for this part ?
Part Number: LM3880 Hi team,
Looking at the LM3880 datasheeet, I see that the Iq is 25 uA which I assume applies when the enable pin is low. What is the current when the enable pin is high?
Regards,
Akash Patel
Part Number: LM3880 Hi
I read the section "Do's and Don'ts" on the datasheet.
It's mentioned that EN do not exceed the threshold before VCC reach the min voltage.
In this case, how is the voltage of FLAG before VCC reach the min voltage? (Low…
#1. there is no Vin pin at LM3880. Do you mean Vcc or Ven. For the Vcc, the input must be within 2.7 - 5.5V. for the Ven, the input shall be greater than 1.v
#2 EN pin has 7uA pull up current.
Regards
Yihe
Hi Ahmed,
Give these files a try, we try to quickly import the pspice file into TINA but it is encrypted in TINA. This should meet your need.
LM3880_TRANS_ENCRYPTED.TSC
TPS2420_TRANS_ENCRYPTED.TSC
Herman
Part Number: LM3880 I have 5 different voltages in y circuit and i need a power on and power down sequence for it since i came to know about LM3880 but i am unable to find current restrictions for example the voltage which i have need to be restricted…
Hi Ahmed, All the available SPICE models can be accessed through the below link. You can look for the models of your interest from there. Thanks, Vivek Agarwal
Hello David,
I have not worked with the LM3880 but it seems like you should be able to use this configuration to enable the module. Was this the setup which caused damage to the LM3880 after several power cycles?
I checked the internal pull-up details…
Part Number: LM3880 Hello,
I have a question regarding the LM3880 PSpice model from TI.
So far, I have been able to downloaded the associated SPICE model, open and view the model, and place the LM3880 part into PSpice. I can run a PSpice simulation…
Part Number: LMZ14201 Other Parts Discussed in Thread: LM3880 Hello
Great to have close all the threads without to have wait a solution
so my situation is still NOT SOLVED
I have test with a buffer transistor ( NPN 4401 ) wit several resistor value…