Part Number: LM3880 Hi, Team,
I have a question for LM3880MF-AE/NOPB.
Is there minimum EN time sepc? My customer is evaluation the device. The device sometimes ignore enable off when the enable is off just a few ~ms.
Best Regards, Satoshi Yone
Part Number: LM3880-Q1 Team,
Is the LM3880QMF-1AE/NOPB logic bearing?
I believe the reason for this question is because if it is programmable then there is a supply chain risk that my customer needs to manage/mitigate.
Thank you.
Part Number: LM3880 Hello E2E,
This datasheet says that this device has 6 sequence type. I can't to found about sequence number 2-6 from orderable device list. Can I request without number 1?
Regards, ACGUY
Part Number: LM3880-Q1 What is the minimum EN low time needed to ensure that the power up sequence is done with the proper timing? In other words, if I have a 10 ms sequence 1 device (timing designator AA) and EN is low for 30 ms to ensure a normal power…
i would recommend figure 20(at page 17) www.ti.com/.../lm3880.pdf . it lists couple ways to solve your problem which is up to whether you want to power up only or both up and down.
Regards
Yihe
Part Number: LM3880-Q1 Hi Sirs,
Sorry to bother you.
Could you help provide LM3880QMFE-1AE/NOPB ESD CDM value for us ?
Thanks!!
ESD-HBM :
ESD-MM :
ESD-CDM :
ESD Report or Evidence (Y/N) :
Pass/Fail :
Part Number: LM3880 Hi team,
In LM3880 datasheet,we specify power on/off sequence in part number, but we can not find the part number and order the samples.
Thanks & Regards
Eddie
Part Number: LM3880 Dears,
I have a customer who used LM3880 encountering some ESD issues.
I was told that It works fine under normal condition. But the LM3880 tends to be a low level with interference, which causes CPU's reset, and the phenomenon…
Part Number: PTH08T240W Other Parts Discussed in Thread: LM3880 I want an LM3880 power sequencer to control PTH08T240Ws connecting FLAG pins to inhibit pins directly. Referring to the datasheet of LM3880, FLAG pins are limited to MAX. 6.0V. But I cannot…
Part Number: LM3880 awg_2v11 pg 22 to 26.pdf
U54 on the first page did not turn on. I believe it follows the recommended circuit exactly (Figure 20). The EN voltage is ~ ground.
Feedback would be appreciated.