Part Number: LM3881 Hi Team The attached circuit shows the connection using the LM3381, with VCC (5V) turned off and the OFF sequence designed. (Because a separate power supply for the LM3881 cannot be provided.)
(1) When the VCC switch is off, and…
Part Number: LM3881 Tool/software: Hi,
I saw in FAQ Cadj min is 200pF and simulation with 1pF
I would like to know if it's possible to use LM3881 without Cadj fitted ?
Thanks
Part Number: LM3881 Tool/software: Hi All,
I have a question about the Adjustable Timing of the TADJ pin. What is the minimum value of the capacitor that can be connected (minimum time)?
Best Regards, Ishiwata
Part Number: LM3881 Tool/software: Dear Support Team,
As part of a reliability analysis based on the VITA 51.1 standard, we are currently collecting failure rate data for components used in our systems.
Could you please provide the following manufacturer…
Part Number: LM3881 Tool/software: Hi
LM3881 enable circuit is described as an internal comparator with precision reference; however in Section 6.5 Electrical Characteristics a threshold precision of 500mV seems to be implied which isn't particularly…
Part Number: LM3881 Tool/software: Hello,
I wanted to have 50us Time Delay between the Each FLAG A , FLAG B, FLAG C.
In the Datasheet no formula is mentioned to calculate TADJ Time Delay. The CADJ capacitor value is mentioned 10nF to have 1.2mS delay…
Part Number: LM3881 Tool/software: Hi TI Team,
Can you confirm the driving capability of LM3881 sequencer for the below scenario
Flag # 1 - # 2 (two) inhibit signal of power supply (LMZ Series),
Flag # 2 - # 4 (four) signals consisting of two…