Part Number: LM393 Other Parts Discussed in Thread: , TL331 , TL331B Team,
Do we have a single channel version of LM393?
Also, what are the differences between LM393 and LM393B?
Thanks
V
Part Number: LM393 Hi expert,
My customer found 6.6us response time and 2 steps output waveform.
Datasheet response time is 1.2us(typ), however waveform show 6.6us.
Could you please let me know the reason of this response time and 2 steps output waveform…
Part Number: LM393 Hi, Could you tell me the input impedance (IN+,IN-) value of LM343? Customers need specific value information for connection and design with other circuits. Regards, Yusuke
Part Number: LM393B Other Parts Discussed in Thread: LM393 , , LM393LV Hi Team,
Our customer would like to know some details about the operation on the newer LM393B compared to the older LM393 specifically if there are any differences in VOL (the small output…
Part Number: LM393-N Other Parts Discussed in Thread: LM393
I want to make sure that the input impedance of the input pins is high enough that it won't be affected by the voltage divider circuit I have designed here in the attached snapshot.
Part Number: LM393 Excuse me,
I am using LM393 to do the OVP circuit and I found a OVP circuit in google and I have some questions
1.) How to calculate the pull up resistor, the pull up resistor is based on the LM393 output sink current? if the output…
Part Number: LM393-N Other Parts Discussed in Thread: LM393 Please answer the following two questions.
①. Please tell me the input impedance and variation of the IN + / IN- terminals. ②. If the input voltage of the IN + / IN- pins is the same (when the…
Part Number: LM393 Other Parts Discussed in Thread: LM5118 , , TLV1702 , LM2903B , I have an application where I'm using the LM393 to compare a constant 12V source and a fluctuating 12V battery. I'm using an LM5118 board as a 12V source(powerboard+), and…
Part Number: LM393 Hi staff
LM393
Input terminal when power is not supplied
1) Is it okay to input voltage to the input terminals (in+, in-) without the power supply voltage of LM393 ? The maximum input at that time is about 5V ?.
2) Will it be destroyed…