Part Number: LM393-N Other Parts Discussed in Thread: LM393 , LM393B Hi Team,
in the face of the shortage of the LM393-N, the LM393P was proposed to me. The replacement can be done without modifying my circuit or the two comparators are perfectly compatible…
Part Number: LM393-N Other Parts Discussed in Thread: LM393
I want to make sure that the input impedance of the input pins is high enough that it won't be affected by the voltage divider circuit I have designed here in the attached snapshot.
Part Number: LM393-N Other Parts Discussed in Thread: LM393 Please answer the following two questions.
①. Please tell me the input impedance and variation of the IN + / IN- terminals. ②. If the input voltage of the IN + / IN- pins is the same (when the…
Part Number: LM393 Hello team,
Is the LM393M/NOPB a drop in replacement for LM393M?
As LM393M/NOPB is old part, w hat is the lifetime of LM393M/NOPB: LM393-N | Buy TI Parts | TI.com ?
Thank you.
Kind regards,
Wouter Kragt
Part Number: LM393-N Other Parts Discussed in Thread: LM393B I have a really specific question regarding the DSBGA packaging for the LM393-N...
There is a customer considering this package, but they are nervous about the way these DSBGA packages have…
Part Number: LM393 Hello Team,
I would like to make sure the LM393 absolute MAX input voltage range.
Our LM393-N data sheet describes as below.
"The input common-mode voltage or either input signal voltage should not be allowed to go negative by more…
Part Number: LM393-N Other Parts Discussed in Thread: LM393 , LMC6772 , TLV1702
Hello, I am using the LM393-N to try to toggle two voltages: Va and Vb. Va should drop high-to-low at V0=1V, and Vb should rise low-to-high at V0=3V. Va changes correctly…
Part Number: LM393-N Other Parts Discussed in Thread: LM393 Hello,
The below application notes recommends to add a series resistance when putting a large capacitance on a comparator output.
http://www.ti.com/lit/an/snoaa35/snoaa35.pdf
Then I would…
Part Number: TLC372 Other Parts Discussed in Thread: LM2903-N , LM2903 , TLV1702 , TLV1822 , LM393 Hi Team,
Do we have an alternative device in DIP package besides the LM2903P?
1) Pin compatibility and the same design, i.e. THT, because we do not want to or…