Part Number: TLV1704 Other Parts Discussed in Thread: TLV1701 , LMV339
Dear Paul, please, report
Sorry, I did not quite understand. I use a non-stabilized 12 V power supply.
1) Can I still apply power to the Vs pin through a passive RC filter (1 kOHm,…
Hello Eggsy,
What are the input signal voltage levels? Are any above 11V? What is the pull-up resistor value?
The LM393 and LM2903 are practically the same. Are they mixing the TI and National (-N) versions?
Part Number: SN74AHC05 Other Parts Discussed in Thread: SN74LS06 , LM393 Dear Team,
we are getting issues with SN74AHC05 IC issues in printer. pls find the below circuit and need your support on this issue.
Issue:
Paper sensor is always detected without…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903 , LM393-N , LM393 , Hi Expert,
I have a question about LM2903 unused pins.
My customers are using only one of the LM2903 2in1, unused part 6PIN = open, 7, 8PIN = GND short circuited.
Customers…
Part Number: LM339A Other Parts Discussed in Thread: LM339-N , TL331 , LM397 , LM393 Hello,
I has to use two of four comparators of a LM339AM in a safety function.
How are the internal circuits an components connectet and there are more components as in the…
Hello Cortland,
Can you provide the full part number that you are using? There are two versions; the LM393 and the LM393-N, the latter being the former National Semiconductor version. They are different "under the hood" and supported by different groups…
Part Number: LF398-N Other Parts Discussed in Thread: UA741 , LM393
Hello, I am working on a project with a boost converter where i need a sample and hold to keep the power value for a short period of time (10 - 50 ms). I have the circuit mounted on a PCB…
Other Parts Discussed in Thread: LM339 , LM358 , LM393-N , LM393 Customer will connect unused channel of LM358 and LM339 (please see below), is this correct?
※VIN+:+15V, VIN-:GND
Customer is already made these circuit, they doesn't want to change as much…
Part Number: LM348 Other Parts Discussed in Thread: UA741 , TLV1702 , LM393 , LM324 , OPA192 , LM358 Hi,
I am currently working on an old design using a LM348N and I am looking to upgrade this chip. I understand this chip is based on the old UA741 which is…
Other Parts Discussed in Thread: LM2903 , LM393-N , LM393 , TLV3402 , TLV3401 , TLV1701 Hello Team,
We understand that LM2903 requires VCC > VICR + 2.0V ( VCC > VICR + 1.5V @ room temp) to guarantee the device operation in full temperature range. I believe…