Part Number: LM4040-N Tool/software: Hello everyone, what is the difference between the two types (LM4040CIM3-10.0 and LM4040CIM3X-10) ? I can't find any difference in the data sheet. Many thanks in advance.
Part Number: LM4040-N Tool/software: Hello Team,
Please provide below details for part LM4040AIM3-5.0/NOPB.
1. Recommended operating temperature
2. Maximum Junction Temperature range
3. Output voltage
4. Maximum and minimum input voltage
Thanks
Part Number: LM4040-N-Q1 Other Parts Discussed in Thread: LM4040-N Tool/software: I'm currently using a zener diode to create a voltage approximately 2.5 to 3 volts below a positive rail, depending on the zener selected. The rail can vary from 11 to 16…
Part Number: LM4040-N-Q1 Tool/software: what is the operating temperature range for the LM4040A41IDBZR. On Mouser, it states -40 to 125 C, but the datasheet does not match that information. Also the datasheet says there is an extended temp range of …
Part Number: LM4040-N Other Parts Discussed in Thread: REF35 , Hi Team,
We are using this 3V Shunt voltage reference IC (LM4040BIM3X-3.0/NOPB) in our design. Our input voltage is 3.3V and desired output is 3V 3mA maximum. Using a series resistor of 100ohm…
Part Number: LM4040-N Hi,
The input voltage is 3.3V and trying to generate a 3V reference voltage for MC Vref.
Our 3.3V voltage range can vary +-5% that is from 3.135V to 3.465V.
Is it possible to use LM4040BIM3X-3.0/NOPB part for our application?
Reg…
Part Number: LM4040-N-Q1 Hi Sir,
Why I did not find the operating temperature range for LM4040QCEM3-2.5/NOPB on the datasheet or website?
Could you share the information with me?