Part Number: LM4040-N Other Parts Discussed in Thread: LM4040 , Hello,
We are looking at the 5V reference LM4040 and had a few questions.
What is the difference in LM4040 and LM4040-N?
Is the LM4040AIM3X-5.0/NOPB the orderable LM4040-N P/N for the 5V reference…
Part Number: LMV358-N-Q1 Hello,
I am looking for CDM value of LMV358-N-Q1, datasheet is not showing the value, I am not sure if TI conducted CDM test for this device or it is just missed to print? Could someone please help on this urgently.
Thank you!
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424 Hi TI Team
May I ask how to calculate the TAS6424 or TAS6584 for the THD+N or THD algorithm?
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hi Expert,
My customer Bosch is using TAS2505-q1 for quite a long time. We are setting bench to test the THD+N EVM on analog input mode and digital input mode.
Analog Input
I do the test…
Part Number: TLV1822-Q1 Other Parts Discussed in Thread: TLV1822 Hi team,
I am just studying TLV1822 (Open Drain output type comparator)
I have found that if Vin+ >> Vin- , then Vout should be high. it means internal fet should be P Type FET or PNP Transistor…
Part Number: LM4040-N-Q1 Hi VRS Team,
I was just wanting to confirm if the tin in the solder on LM4040QCEM3-2.5/NOPB is Matte or Bright? We’re using it on an upcoming project and I’m going through potential tin whisker mitigations.
Best Regards…
Part Number: LM4041-N-Q1 I am using LM4041QEEM3-1.2/NO regulator to get 1.2 volt output. But when checked it with no load condition it's giving me 1.4 Volt output an with 15 mA load it is giving me 0.8 Volt output. My Rs value is 47 ohm. Please suggest…
Hi Xiaxiang,
Xiaoxiang Liu said: DOUT+ and DOUT- are connected according to the correct cable sequence, but it doesn't work.
Can you clarify what you mean by correct cable sequence?
Please share additional information:
1. Can you share the schematic…