Part Number: LM4041-N I have been trying to use the LM4041_NA1P2_TRANS in PSpice and it seems like the device only regulates if the "annode" is connected directly to ground.
I found multiple forums that brought this issue up, but there was never any…
Part Number: LM4041-N Other Parts Discussed in Thread: LM4051-N Hi,
I am considering a simple current source design (Iout smaller than 100mA from a 5V power supply) using either LM4041-ADJ or LM4051-ADJ, since their Vref is defined between the cathode…
Part Number: LM4041-N-Q1 Other Parts Discussed in Thread: INA228 Tool/software: Hi Sir,
I want to design current source as below for LM4041. This schematic from LM4041 datasheet.
1) May i use the MMBT3906(package SOT23) to replace 2N2905 and 2N3964…
Part Number: LM4041-N Tool/software: Hi team,
We want your opinion about below added explanation in new revision detasheet of LM4140-N.
"When the output voltage, VZ, is set below 2.5V on adjustable versions of LM4041-N and LM4041-N Q1, the device…
Hi Maia,
Depending on the circuit design, it could be helpful to have an option such as LM4041-N.
One example is when designing a current source. LM4041-N ADJ is an ideal solution in current sourcing because its feedback voltage on FB is with respect…
Part Number: LM4041-N Dear Team,
Our customer is using LM4041CIM3X-ADJ/NOPB at mass production. however, it's old device.
they would like to replace new device in the future project if we have.
Best Regards,
Seijiro Matsuoka
Part Number: LM4041-N Tool/software: Hello
what is the difference between the below 2 P/Ns?
LM4041DIM7-ADJ/NOPB vs LM4041DIM7 X -ADJ/NOPB
according to the datasheet, there is no difference
Tks
Part Number: LM4041-N-Q1 Other Parts Discussed in Thread: LM4041-N Tool/software: I'm trying to build a current source circuit (for small currents in 5uA range) and I found that I can use lm4041 adj with 2 pnp transistors to build it. (2n2905 & 2n3964…
Part Number: LM4041-N Hello, What is the difference between a LM4041AIM3X-1.2/NOPB and LM4041AIM3-1.2/NOPB (no X)? Is it just the lead finish? In a previous post they showed the reel size was different but these are both 3000.
Thank you,
Tanya Va…
Hi Jayden,
Although an output capacitor is not necessary for LM4041-N-Q1, any typical capacitor value between 0.1uF to 10uF should work fine.
Thanks, Joshua