Part Number: LM4050-N Team,
Can you answer the following?
I have a question about TI’s LM4050 (5V Zener Shunt) reverse current transient rating. The abs max information in the datasheet specifies 20 mA reverse current rating, but can the part exceed…
Hi,
LM4050-N-Q1 has a reverse current range of 60μA minimum and 15mA maximum, so it will likely not be suitable for this application requiring between 40mA and 350mA. We have a newer device, LM4060, but this device supports only 50μA to 50mA.
I have…
Part Number: LM4050-N In the existing design, LM4050AIM3-5.0 is used. Since this part is discontinued, we are planning to use the alternate part LM4050AIM3X-5.0/NOPB. I understand that the older part has lead finish wheras the NOPB is ROHS compliant part…
Part Number: TINA-TI Other Parts Discussed in Thread: LM4050-N , TINA-TI I am looking for a simulation model for LM4050-N in the 5 Volt Variant ( www.ti.com/.../LM4050-N ) and found a reference design: www.ti.com/.../snom432 and a model: www.ti.com/.…
Part Number: LM4050-N Hello,
In order to calculate the failure rate of products using this part, could you please provide information on the failure rate of the LM4050BEM3-2.5/NOPB, as well as MTBF and FIT values?
Thank you,
Keisuke IKEMORI
Part Number: LM4050-N Tool/software: Hello,
I see that LM4050 Q AEM3-8.2/NOPB is obsolete with LM4050AEM3-8.2/NOPB as the recommended pin-to-pin alternative.
Is there a datasheet for the obsolete LM4050 Q AEM3-8.2/NOPB? I do not see this MPN listed…
Part Number: LM4050-N-Q1 Could you please help confirm below two questions? Thank you!
First please check and confirm below products are NOT subject to China’s dual-use regulations.
Second please check and confirm that Chinese-made synthetic diamonds…