Part Number: LM4050-N Team,
My customer has a question regarding the LM4050 (5V Zener Shunt) reverse current transient rating. The abs max information in the datasheet specifies 20 mA reverse current rating, but can the part exceed this for short transient…
Part Number: LM4050-N-Q1 Hi team,
Could you pls help share below Ir=1mA is spec at what temperature range? Datasheet has list 25C and full temp range spec for Ir=100uA, but didnt specify it clearly for Ir=10mA/1mA
Thank you
Scarlett
Part Number: LM4050-N-Q1
Hi Expert,
My customer is doing the FuSa analysis for their system. LM4050 is used in this project. Can you help fill the component type to the excel for LM4050 based on SN29500?
I saw there have SN29500 category in FuSa…
Part Number: LM4050-N-Q1 Hi Team,
Figure 14 of the datasheet of LM4050QML and Figure 43 of DAC121S101WGRQV show that it can be used as power supply and reference to ADC128S102QML and DAC121S101WGRQV . Our customer would like to know how many ADCs or…
Part Number: LM4050-N-Q1 Other Parts Discussed in Thread: TL431 , Dear team,
Before TL431 have requirement for the Cload. I am not sure whether our 4050 have the same requirement. Below schematic, Rs=49.9k and C94/Cload=0.001uF, is this ok?
…
Part Number: LM4050-N-Q1 Dear team,
For this device, there is no output capacitor required. If the customer wants to add capacitors to reduce noise, is there a maximum capacitor limit?
Thanks & Best Regards,
Sherry
Part Number: LM4050-N-Q1 Hi,
i looked into the LM4050-N-Q1 data sheet ( https://www.ti.com/lit/ds/symlink/lm4050-n-q1.pdf ) page 5:
is it really 1024mV tolerance?
Thank you
Hi Experts,
We would like to ask your assistance on this query from a client as per this thread's title.
There is a customer who has been using the LM4050AIM3-2.5/NOPB (from National Semicon) part for years but turns out to be out of stock, planning…
Part Number: LM4050-N Hi
Our customer found a sample which has low accuracy at low temp. (Please see the following temp.)
Vs=8V, Vout=5V, LM4050AIM3-5.0
1. Do you think that accuracy of a failure sample is not normal at low temp?
2.Is…