Part Number: LM4128 Other Parts Discussed in Thread: REF4132 , REF2033 Tool/software: I'm considering LM4128's enable pin control by logic IC. I want to know LM4128 enable pin's input impedance or input leakage current.
Please let me know. Best regards…
Part Number: LM4128 Other Parts Discussed in Thread: DRV8874-Q1 , Tool/software: Hi,
Our customer has requested the Ψjt parameter.
Can TI provide this parameter?
They are using this product with DRV8874-Q1 and are estimating Tj with Ψjt, so it would…
Part Number: LM4128 Tool/software: Due to an unfortunate small mistake, we have fifteen (15) different LM4128CMF-3.3/NOPB outputs connected in parallel (to the same net: 3.3 V). All the LM4128CMF-3.3/NOPB outputs are connected together (the pin 5 of all…
Part Number: LM4128-Q1 Tool/software: Hello,experters
when I use to LM4128-Q1,as below,IO power of enable pin input level is same as VIN voltage or any input level is ok.
In the datasheet ,I can not see to relation to enable threshold level of rising…
Part Number: LM4128 Hi All,
I have a question about LM4128.
Maximum VIN is listed.
However, the minimum value is not specified. What is the minimum VIN value?
Also, what is the EN condition for VIH min =65%?
For example @EN=3.3V etc.., …
Part Number: LM4128-Q1 Other Parts Discussed in Thread: LM4128 , REF4132 Hi Team,
My customer is requesting if TI could provide a spice model for this device.
Thank you.
Regards, May
Part Number: LM4128 Hello all, I have a high end military customer requesting the number of transistors in the LM4128 device.
Is this information you can provide?
Please advise.