Part Number: LM43601 Hello,
I use the LM43601 simple switcher in many designs.
I've selected this component because of its EMC and low current performances.
It works fine when supplied by a 15V source.
When my system goes in standby mode, the LM43601…
Other Parts Discussed in Thread: LM43601 I would like to confirm Drop-out curve of LM43601.
Do you have the data of drop-out curve with temperature-dependent change?
If you don't have it, how does the characteristics change by the temperature?
Best…
Other Parts Discussed in Thread: LM43601 Hi,
I've made a design with an LM43601.
Input voltage is 15V and output voltage should be 5V.
I've taken the values recommanded by the datasheet for resistors, capacitance and inductance (except output capacitor…
Other Parts Discussed in Thread: LM43601 I would like to confirm IQ for LM43601.
In the datasheet, there are specifications and data for 3.3V output voltage.
Do you have the data for 5V output voltage?
Is the value of IQ depend on output voltage?
Best regards…
Other Parts Discussed in Thread: LM43601 i would like to confirm soft start for LM43601.
1. Which is correct 3.86ms typ.(datasheet P6) or 4.1ms typ. (datasheet P18)?
2. Do you have the data for the variation of soft start time (min/max)?
We don't need…
Other Parts Discussed in Thread: LM43602 , LM43601 Hi there,
I have a customer working on a design with our LM43601 and LM43602 parts, whom I am trying to support. Can someone confirm that I am reading the datasheet correctly please?
Looking at page 30…
Other Parts Discussed in Thread: LM43601 Hi,
I am designing a 24V to 5V Buck Regulator using LM43601 @ 1A .
While calculating the Output capacitor value using the formula given in datasheet i got value of around 100uH. But when i use the formula mentioned…
Other Parts Discussed in Thread: LM43601 I would like to confirm ESR of the output capacitor for LM43601.
ESR has the frequency characteristics.
Could you please teach how much the frequency for the caluculation is?
I think we should use the ESR value…