Other Parts Discussed in Thread: LM43602-Q1 , LM43601-Q1 Hello,
The Voutp-p simulation result of LM43602-Q1, LM43601-Q1 on Webench was about 100mV~120mV. Is this result correct? I think that this is error in webench. If yes, could you please correct the Webench…
Other Parts Discussed in Thread: LM43601-Q1 Hi
I have a question about LM43601-Q1.
In the datasheet LM43601-Q1 page 1,
About 600Mhz Emission level increases suddenly as shown above.
Do you know why did suddenly emission level increase in the near 600Mhz ?
…
Other Parts Discussed in Thread: LM43601 Dear All
Would you give below HS FET and SW pin parameter of LM43601 for noise simulation? A rough estimate would be fine with us.
・Input capacitance of HS FET
・Output impedance of SW pin
・Parasitic capacitance of SW…
Hello Alessio,
As you pointed out, the whole semiconductor industry is impacted right now so certain chips are hard to come by.
I don't have any information regarding future availability of the LMR50410/LMR14010, but the following devices have availability…
Other Parts Discussed in Thread: LM43601 Tool/software: WEBENCH® Design Tools Hi,
I am just getting to know your tool: Webench power designer. I have tried out a few simulations and exported a PDF design report. At the bottom of this there is a master…
Hi John,
Some supplementary information which may be useful.
1) It seems that I can repeatedly re-run PSpice so long as I don't turn off the PC but maybe that's just because the power cycle causes it to automatically update.
2) Below is a screen…
Part Number: LM43601PWPEVM Other Parts Discussed in Thread: LM43601 Tool/software: WEBENCH® Design Tools Hello,
I have designed -5V 0.3A inverter circuit with using WeBench software. The output file is also attached to this post. Based on the WeBench…
Part Number: TPS40170 Other Parts Discussed in Thread: LM73605 , LM43601 , TPS54541 Hi Ti family.
In my design there will 4 different voltage levels.
Voltage input: 11V to 24V but for safety max will be more than 30V. ( transients)
Outputs:
1.2V 8A / 3…