Part Number: LM43602 Hello,
i want to use the SON Package, but in the Datasheet there are no information about that package and i found nothing on " www.ti.com/.../searchtipackages.tsp for Package Drawing DSU.
Best regards
David
Part Number: LM43602 Other Parts Discussed in Thread: LM20333 Tool/software: WEBENCH® Design Tools When opening the design with the required values (VSON package, 5.95V≤Vin≤27.6V, Vout=5.12V, Iout=1A, 30°C), Webench simply states that this is not possible…
Part Number: LM43602 Hello,
Regarding to enable level on LM43602, my customer is asking a question.
According to datasheet page 5, VEN-VOUT-H is 2.2V(typ).
But according to datasheet page 14, VEN-VOUT-H is described the following.
The LM43602 switching…
Part Number: LM43602-Q1 Hello,
Would you let me know how the equality 19 and 20 in the datasheet shown below were derived?
Or make a brief explanation about what is compared to what in these inequalities?
One of my customers is making a lot of trouble…
Other Parts Discussed in Thread: LM43602 Hello,
LM43602 supports low dropout operation by frequency foldback.
The eventual (low end) frequency seems dependent on the current as shown below.
What does determine the eventual frequency?
Thanks.
Oguri (TIJ…
Other Parts Discussed in Thread: LM43602 , LM46002 Good day Colleagues,
My customer made the same schematics as app note says for the LM43602 to operate as negative regulator.
He has an issue during startup. Not every time, but often. He applies input…
Other Parts Discussed in Thread: LM43602 Hello,
We need to delay the power up of LM43602 switching regulator by ~1 sec. Can we use an RC of 500K & 10uF on "EN" pin ?
Will there be any latch-up issue on LM43602 during turn-off sequence ? Suppose…
Other Parts Discussed in Thread: LM43602 Hi all Would you mind if we ask LM43602? The data sheet shows the Vin-min condtion which is "Vin-min = Vout / (1 - (Fs * Toff-min))". Of course, we recognize there is the duty limitation as above. On the other…
Other Parts Discussed in Thread: LMR23625 , LM43602 Hi all Would you mind if we ask LM43602 and LMR23625? We'd like to realize the following spec using LM43602 or LMR23625. -Vin=12V, Vout=-12V, Iout=0.8A We guess that it is possible. Is our recognition correct…
Other Parts Discussed in Thread: LM43602 Hello,
In a condition of Hi-Vin, Lo-Vout, and Hi-Fsw, LM43602 may not meet the specifications in the datasheet.
I guess, the device may skip switching cycles to realize necessary duty cycle.
Is there any known…