Part Number: LM43603-Q1 Using LM43603-Q1 as 15V to 9V converter. I have a external 5V supply available and using this for Bias rail per datasheet recommendation.
The 5V rail can be present before /after the 15V.
It mentions in the datasheet that Bias…
Part Number: LM43603 The LM43603 (exact part number LM43603PWPT) datasheet says that the CCM Mode:
Output voltage ripple will be at a minimum in this mode and the maximum output current of 2 A can be supplied by the LM43603.
This is a 3A part. Should…
Part Number: LM43603 Dear TI Team,
We would like to seek your confirmation regarding the LM43603PWPR parts with DC2603+ date codes.
During our inspection, we observed that the solder coverage on the thermal pad did not exhibit continuous, defect-free…
Part Number: LM43603 Current circuits use an external RT resistor with a resistance value of 89k ohm (tolerance +/- 0.5%) to determine the switching frequency. The maximum switching frequency range is calculated from 401.8kHz to 495.99kHz using the maximum…
Part Number: LM43603 Hi team,
It is recommended that 0.47uF for bootstrap capactior. Is it possible to use larger cap like 1uF for bootstrap? Best regards, Goto
Part Number: LM43603 Hello guys,
One of my customers is considering using LM43603 for their next products. They are simulating LM43603 with Webench. At this moment, they have the following questions. Could you please give me your answer to the questions…
Part Number: LM43603 Tool/software: Hello,
Before 2 years we developed a new device with LM43603. The design was done with WEBENCH Designer. Input voltage 12-28VDC, output voltage 5V, Iout - 3A max., Cout 180uF polymer organic capacitor, RT - 115kOhm…
Part Number: LM43603
I have made 2 PCBs with the same schematic shown but different layouts. One circuit works fine and the other has poor output voltage regulation.
On the one that has poor regulation, under no-load it outputs the desired voltgae…