Part Number: LM43603 Other Parts Discussed in Thread: LM61440-Q1 Just received word that there can be some inrush issues if there isn't some matter of "slow start" for the LM43603 converter. It takes some time 't' to rise for a soft/slow start, but there…
Part Number: LM43603 Hello guys,
One of my customers is considering using LM43603 for their next products. They are simulating LM43603 with Webench. At this moment, they have the following questions. Could you please give me your answer to the questions…
Part Number: LM5576-Q1 Other Parts Discussed in Thread: LM5576 , LM43603 Hi,
I Want to use the LM5576/-Q1 for a new project,
Input voltage: 45-75V
Output voltage: 38V
Current: 2.4A, in ambient temperature of 85 degrees Celsius
I can't find in the datasheet…
Part Number: TPS57160-Q1 Other Parts Discussed in Thread: TPS62821 , TPS54160 , LM43603 Hello,
my customer evaluated the TPS57160 using the TPS57160-Q1EVM in which they modified the following: R3, R4 = DNP; R7= 16k; R8=5k2.
Their requirements were the following…
The LM46001-Q1 has the same package as the LM43603, which has landing pattern on its DS.
www.ti.com/.../lm43603.pdf
I will send request to update the LM46001-Q1 DS with landing pattern attached.
Thank you,
Yang
Hi Priyanka,
So you want a DCDC with watchdog built in which could communicate with an external MCU, right? To make the DCDC more reliable or the MCU?
For a more reliable DCDC, some DCDC part has a "Powergood" function, like LM43603-Q1 . But…
Other Parts Discussed in Thread: LM43603-Q1 HI,
I use the webench to have a recommended circuit whit simulation of the LM43603-Q1. My main entry is 12.3V for Vin Min, 16 V for Vin max et 5V@2.3A for the output. For that, I got a value of 1 MOhm Rfbt and…
Part Number: LM22670-Q1 Other Parts Discussed in Thread: LM22670 , , LM43603 Dears,
I can't found the LM22670 have short protect function on the datasheet, its only have the frequency current foldback mode, If the circuit is still on short status and…