Part Number: LM46000 I have a customer who has some questions regarding the operation of the LM46000.
I have a lot of information that I can send, but I cannot post it here in the forums. Can I send it directly to you to look at? I reall need for you…
Part Number: LM46000-Q1 Hello team,
Hope you are doing well. Customer is using LM46000A-Q1 in their design and tested the part for 1KV/-1KV. The part did not pass as per the ratings in table 6.2 ESD ratings. Customer is asking if we can verify this…
Part Number: LM46000 Hi,
Typical values of the external components are written in Table 2 of the data sheet.
I would like to know the recommended values of L, C and R under the following conditions.
■Use conditions ・Vin=20-36V ・Vout=19V ・Iout…
Other Parts Discussed in Thread: LM46000 Hi Sir
Our MM customer Gogoro is design LM46000, however they checked LM46000 datasheet does not find Ipeak-min in our spec. also they measured Ipeak is not constant .
Thanks.
Below is 51Vin and 20Vin No…
Part Number: LM46000-Q1 Dear all.
There is mention of the A version in the datasheet of LM46000-Q1. The RPGOOD value and optimized for PFM are caught in the difference in A version. What is the point where PFM was improved?
Regards, PAN-M
Other Parts Discussed in Thread: LM46000 I'm trying to use the LM46000 to generate ~11V from a nominal 14.4V supply.
The has some switching action happening, but the switch pin doesn't 'appear to swing to Vin or Gnd like I would expect.
The output…
Other Parts Discussed in Thread: LM46000 Want to control the Enable Pin of the LM46000 over external logic. During power-down the Enable voltage could be higher then the Input Voltage. It seemed, that there is a Diode between Enable-Pin and Input-Pin…
Other Parts Discussed in Thread: LM46000 Hello,
I hope someone can help with this. I'm using the LM46000 to produce a +3.8V output from an input range of +5V to +30V. If Vin starts fairly low (say 7-8V) the circuit sticks in PWM mode and its current…
Part Number: LM5165-Q1 Other Parts Discussed in Thread: LMR36503-Q1 , LM46000-Q1 , TPS57060-Q1 , LMR36500 , LMR36503
Hi TI Team,
We plan to use this device (LM5165-Q1) in a 24 V automotive application with a 5 V output . The expected load is ultra…
Part Number: LM46001 Other Parts Discussed in Thread: LM46000 , We have an a few percent of boards failing in the field in the same way as described in the related thread. It appears that the ability for VIN to provide the initial voltage to the LDO in…