Hello,
1. For the pin to pin components, the LM2594HV will be your best option. If you have the ability to re-layout the board, you can also look at the LM46000: www.ti.com/.../lm46000.pdf
2. The necessary filtering for the DC-DC will depend on your…
Part Number: TPS54340 Other Parts Discussed in Thread: LM46001 , LM46000 , TPS54060A , TPS54160A , LMR16006 Hi,
I am considering an inverting circuit with the following specifications. There is PMP4369 in the reference design, but is it possible to adjust…
Hi,
It should not be, but you have to make sure that the voltage never reaches beyond the ABS max of the device, especially during transient. If i would choose, i would choose a 60V device such as LM46000 or LM46001. It is a synchronous part therefore…
Other Parts Discussed in Thread: LM46000 Dear sir,
When I use LM46000 webench to design my circuit, I edit the design circuit.(not component value)
After that, how can I find the bode plot? It seems only can know waveform.
Thanks for your help!
Regards…
Other Parts Discussed in Thread: LM5574 , LM46000 Please let me know about two points below of LM5574 maximum rating.
①Is there spec information of SW to GND transients?
For example, LM46000 datasheet page-4 described "SW to PGND less than 10ns Transients…
LM46001 looks very interesting for us. I have ordered the evaluation Module to test the switcher. There is also a 0,5A version LM46000 available. Is there a difference according the radiated emission whether we use LM46001 or LM46000 each with 0,5A output…
Other Parts Discussed in Thread: LM46000 , LM46002 I am looking for a synchronous buck converter with high efficiency.
In the past the customer I used the TPS54061 but the current output is too low for my new application. The 0.5A version of the part ( T…
Other Parts Discussed in Thread: LM46000 , LM5017 Hi,
While configuring buck into IBB, it is generally suggested to keep one by-pass capacitor from input to output.
My concern is, if capacitor is connected from vin to vout, Line transient will be worsen…