Part Number: LM46001-Q1 Hello,
I have a question regarding the current consumption of the LM46001-Q1 @ no-load.
The datasheet indicates a typical operating quiescent current of 24uA under certain test conditions. In our application, the current consumption…
Part Number: LM46001-Q1 Hi team.
I ask about the Hiccup mode when PGOOD is floating.
I checked about hiccup mode at datasheet(7.3.12 Overcurrent and Short Circuit Protection)as follow.
'Hiccup is only activated when the power-good flag is low.'…
Part Number: LM46001-Q1 Hi team
The customer requested a solution for the following:
1. When Input voltage is UVLO, can output is cut off by using PGOOD pin?
If possible, please let me know the application.
2. When output voltage is UVLO, can output…
Part Number: LM46001-Q1 Other Parts Discussed in Thread: LM46001 Hi Team
The customer used the LM46001 to configure the environment below.
1. Vin : 18 ~ 36V (Typ : 24V)
2. Vout : 5V
3. Imax : 1A ( I_continus < 500mA)
The circuit configuration was based…
Part Number: LM46001-Q1 Hello,
We use LM46001-Q1 for 24 to 12V conversion @ current 500mA. SW FRQ is 500KHz. In conducted emission testing we are getting peak @ 49dBuV. This we are not able to suppress at any combination of CLC filter at input side regulator…
Part Number: LM46001-Q1 Other Parts Discussed in Thread: TPS568215 oIn the thread TPS568215: FB terminal control by external is an application to controll the output voltage via DAC/CPU or FPGA and a LPF.
We want to use the LM46001 . The CPU generates an…
Part Number: LM46001-Q1 Other Parts Discussed in Thread: LM43603 Hi TI Support, We are using LM46001-Q1 step down voltage conerter. But in data sheet there is no PCB Layout land pattern for this part. Kindly provide us the land pattern for above mention…
Part Number: LM46001-Q1 Other Parts Discussed in Thread: LM46001
Hello,
is there an EMI disadvantage when using the LM4600x in DCM instead of CCM? CCM is FPWM right? So CCM should be better regarding EMI compared to DCM.
Can the circuit be tweaked (switchin…
Part Number: LM46001 Hello,
Could you please submit IMDS report for below components to Kimball Jasper IMDS account 15918. Those are urgently needed for IMDS for ZF and Knorr Bremse application.
Kimball Part#
Supplier name
IMDS Status
MPN
…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM46000-Q1 , LM5176 , LM46000 , LM46001 Dears,
I'd like to request the schematic review of BMS application included LM5176-Q1, LM46000-Q1, and OPAMPs.
The application details are as follows.
If…