Part Number: LM46002-Q1 Hi community,
is there any information about the behavior of the LM46002-Q1 if the input voltage falls below the desired output voltage. This happens for example during cranking of an engine. In this case the input would be ca…
Other Parts Discussed in Thread: LM46002-Q1 , LM46002 Hi,
My customer has question about LM46002-Q1. Could you tell me about questoin?
[Question] - How much is the variation of switching frequency at over temperature under the following condition?
Rt=17…
Part Number: LM43603-Q1 Other Parts Discussed in Thread: LM43603 , LM46002 We are having startup issue with using an LM43603 rather than a LM46002. Schematic below.
When the supply has around 6V to 8V at the input the output ripple is around 400mV. When…
Thanks for the clarification Mohit. The LM46002-Q1 can meet the following requirements, not the LM46001-Q1 (due to the impact of topology modification). I can also recommend the following Module for the negative rail: LMZ34002.
Regards, Alejandro
Part Number: LMR34215FSC5EVM Other Parts Discussed in Thread: LM46002-Q1 Hi Team,
My customer is working with the LMR34215FSC5EVM and without load is measuring input current of 24mA. Could you please help us understand why? The datasheet Iq of 24uA was…
Part Number: LM5575 Other Parts Discussed in Thread: LM46002 , LM5164-Q1 , LM5164 I've used Webench for the following design:
24V In
-17V Out @ 0.5A
500kHz switching frequency
The Webench design did not include the snubber R/C that datasheet and eval…
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6505B , SN6505A , SN6505BEVM , ISO1042 , LM46002 Hi expert,
Now SN6505 is under evaluation on customer side. The competitor is CF0505XT and CWRF1215S. Those two device are all integrate transformer…
Part Number: TPS62810-Q1 Other Parts Discussed in Thread: LM46002 Hi,
I understand that the PG only responds to a variation of the voltage regulated downwards. Consequently, if the voltage rises in a worrying way, I could not know this by only monitoring…
Other Parts Discussed in Thread: LM46002 , LMR33620 , LMR33630 , LMR36006 , LMR36015 , TPS62130A-Q1 Hi sir,
Customer used LM46002 in other projects, but now they would like to look for similar solution but need to meet Cispr25, could you help to suggest? If…
Other Parts Discussed in Thread: LM46002 , LM43601-Q1 , LM43602-Q1 Hello,
I can not find a recommended footprint for the LM46002 which comes in a HTSSOP-16 PWP package (TI drawing number R-PDSO-G16). Please help.
Thanks!