Part Number: LM4766 Other Parts Discussed in Thread: TAS5825M , TAS5828M LM4766 is very old material, Will there be an EOL plan?Any new replacement materials?
Part Number: LM4766 Other Parts Discussed in Thread: LM3886 , I am familiair with the LM3886, it hat a minimum loop gain requirement of Au=10 for stabillity
I am exploring the posibillity to design a bridged compound amp with the LM4766, so i can freely…
Part Number: LM4766 Hi, Good day. Our customer has this question regarding the LM4766. Can you please help us clarify? Thank you. I want to set the circuit up in bridged mode however. the data sheet shows pins 6 and 11 tied to -VEE whereas VCC is not…
Part Number: LM4766
Hi, Good day. Our customer wants to simulate the LM4766 using Pspice for TI however they face an error that states "Subcircuit LM4766_0 used by X_U1 is undefined". COuld you please help us on how to fix this issue. I appreciate your…
Part Number: LM4766
Hello,
We use the LM4766 in bridged mode as a driver for the coil of a linear motor. The coil has resistance of 33 Ohms and an inductance 62 mH. In some cases, we connect two motor coils in parallel. So we have a R L of 16…
Part Number: LM4766 I designed a stereo audio amplifier using the TI LM4766 and I’m seeing noise riding on top of the sinewave. Please see attached pictures (no noise, noise, noise plus clipping). This is a single ended, stereo (2x20W), 42V rail amplifier…
Hi Derek,
no, because I can listen a beep from the LM4766 if my input amplitude is high enough. Should the gain nearly linear to the input?
Regards,
Lukas
Part Number: LM4766
kai klaas69 very kindly provided me with data and analysis regarding the LM4766 Amplifier section of my circuit.
e2e.ti.com/.../877048
Now that I have modelled the circuit with components, is it possible that it could be thoroughly…
Part Number: LM4766
Kai, kindly answered my query regarding the use of LM4766 as an Ampifier using the link attached.
He stated "You can close S1 permamently, if you don't want to mute the LM4766 by hand." As he did not offer a value for Cs, may it…