Other Parts Discussed in Thread: LM48310 Hi,
I am using a LM48310 ultra low emi audio amplifier and I am having two issues. They are:
1) Radiated emi in the 2.4 ghz band
2) When output is shorted either to ground or the speaker outputs are shorted appears…
Hi Aaron,
Thanks that would be great.
I also had a quick comparison to other TI class D amplifiers that have similar maximum output power rating. (i.e LM48310 or LM48312 ) and the efficiency for the TLV8320AIC3100 amplifier is significantly worst at the…
Part Number: TPA2005D1 Other Parts Discussed in Thread: OPA1604 , , TPA6211A1 , TPA2025D1 , TPA2080D1 , TPA6205A1 , LM48310 Hi,
I am using, OPA1604 high performance audio op-amp, (soundplus series has very less THD and noise figure). Next stage is audio amplifier…
Other Parts Discussed in Thread: TPA2013D1 , LM48310 Hello All,
I need some opinions, and/or advice.
I am designing an audio amplifier that has around 2.5W per channel. But I want it to be powered from Li-Ion batteries. I have 2 ideas.
Idea 1; use a …
Other Parts Discussed in Thread: TPA2005D1 , LM48312 , LM48310 I need an audio amp, mono, that can drive up to 50mA into a 2.3ohm custom speaker, (115mV). VCC will be 3.45V-3V. Analog input will be centered at 1.25V
This is a battery powered device so it needs…