Part Number: LM48580 Hi,
we have found an error in our schematic using the LM48580. In the datasheet, we didn't see that the device can only be used with ceramic speaker.
We took a magnetic one:
https://www.knowles.com/docs/default-source/model…
Part Number: LM48580 Hi TI,
I have a problem when the LM48580 is enabled by the SHDN Pin, but no input over IN+ is done. We are using a Timer of a µC with a PWM which is output to IN+. When no PWM is played and the IC is "ON" than at OUT+ and OUT- I…
Part Number: LM48580
Hi, Team,
Customer demand is 100mW THD +N <1%)@ capacitive load, single channel, differential output, for a voltage-driven MEMS speaker. Please help to recommend us the most suitable device
Thanks
Part Number: LM48580 Hi Sirs, The Vin (max) of the LM48580 is 3Vpp (~1.060Vrms) according to the datasheet page 5. In case of 5V VDD, will it damage the LM48580 device or just generate output clipping when the input voltage exceeds 3Vpp since the absolute…
Part Number: LM48580 Hi Sirs, There is a 10ohm current limit resistor with the LM48580 reference design (datasheet page 1), while the 10ohm resistor can impact efficiency and generate heat. Would you please advise the minimum load resistance with this…
Part Number: LM48580 Other Parts Discussed in Thread: LM48560 Greetings,
I have an application where I need to drive a piezo from two sources:
-Normal operation where input is driven by standard audio source.
-Secondary backup operation where…
Part Number: LM48580 We are using an LM48580 to drive a piezoelectric speaker, measuring the power supply pin of 48580, 48580 will bring relatively large ripple to the power supply, the peak value is about 900mv, there is no problem without a buzzer,…
Part Number: LM48580 Hi E2E,
Good day. Our customer is using the LM48580 and would like to achieve a +30V output. However, when they check the output signal, the output is 30 Vp-p but from -15V to +15 V. How to configure the device to achieve the +30V…
Part Number: LM48580 this is our Piezoelectric speakers Part number BPR2207H0-F2,I use a lithium battery to power the evaluation board 48580 and then add an audio signal to the 48580 signal input. The piezoelectric speaker is connected directly to the…